Question
FMC: How to get full memory access on a 32 bit SDRAM via 16 bit data bus?
1)STM32H745I-DISCO, the bus is 16bit and the memory is 32bit.
In the spec there is 128M-bit SDRAM.
Question is if full memory 1(28M-bit) is available for usage on this kit?
2) If answer is yes on first question. We can only access half of the memory and we don't understand why. Adress pin A11 never goes high. We have similar SDRAM ( issi 32-bit ) and STM32H750 via 16bit data bus. Question is how to configure FMC to access 32 bit SDRAM via 16 bit bus.