Skip to main content
RLee.7
Associate
Sep 18, 2019 6:25 AM UTC
Solved

FMC controller conflict issue

I have 2 FMC controllers on my STM32F429 design.

  1. The first controller is SDRAM controller which is used by LTDC&DMA2D as video buffer;
  2. The second controller is PSRAM controller which is used as data interface between STM32 and FPGA;

​

The two controllers works well individually. However, when I enable them at the same time, the PSRAM controller stops working and even the Keil crashes. I guess the SDRAM controller may have conflict with PSRAM controller, so I shut the SDRAM controller and LTDC/DMA2D before use PSRAM, but the issue still happns sometimes.

 //shut down SDRAM related modules
 HAL_DMA2D_Suspend(&hdma2d);
 HAL_LTDC_DeInit(&hltdc);
 HAL_SDRAM_DeInit(&hsdram1);
 HAL_Delay(1000);
  
 //use PSRAM interface to read FPGA data
 memcpy(rd_buf, (uint16_t *)FPGA_DAT_ADDR, rd_bytes); --Crash here!!
 
 //turn on SDRAM related modules again
 HAL_Delay(1000);
 if (HAL_LTDC_Init(&hltdc) != HAL_OK)
 {
 Error_Handler( );
 }
 HAL_DMA2D_Resume(&hdma2d);

I've set breakpoint to ensure the rd_bytes value is correct. Also, I've caputured the signal wave on the FPGA side and the result was that FPGA runs out of data but PSRAM controller still set PSRAM NE signal valid.

Can someone give me a clue on how to debug this issue? Thank you.

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Sep 18, 2019 6:56 AM UTC

Erratum FMC dynamic and static bank switching?

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
Sep 18, 2019 6:56 AM UTC

Erratum FMC dynamic and static bank switching?

JW

RLee.7
RLee.7Author
Associate
Sep 18, 2019 11:10 PM UTC

Thanks Jan,that's what exactly I need.