Skip to main content
yonatan
Associate III
May 20, 2025 2:45 PM UTC
Question

FMAC implementation

Hi all

I have an IIR filter design with 7 coefficients. (For feed-forward and for feed-back)

Regularly all the coeffs are between -1 to +1

So I Just multiply each by 2^15 to get it in q1.15 format.

However, now, the feedforward coeffs are very small (0.0000000001 or something like that)

and the feedback coeffs are up to 30.

How to initialize the system to get it work?

This topic has been closed for replies.

6 replies

Pavel A.
May 20, 2025 8:34 PM UTC

Is chatgpt broken today?

 

yonatan
yonatanAuthor
Associate III
May 21, 2025 5:37 PM UTC

Seriously?

I was thinking that the toxicity is only stack-overflow privilege.

Do you really want me to go through all the BS it gives me just to get the conclusion

that I need to scale the factor to get them in values greater than 1 but

it is impossible due to the fact they are TOO SMALL (as I said in the post)

Take a look here:

https://chatgpt.com/share/682e0de8-9490-800a-9a07-e690a4711dc9

 

Tesla DeLorean
Guru
May 21, 2025 8:30 PM UTC

Fixed point probably not going to cut it then, could you use the FPU and VMLA.F32, with 32-bit floats?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
yonatan
yonatanAuthor
Associate III
May 25, 2025 2:32 PM UTC

That's what I doing right now. with a for loop...

gregstm
Senior II
May 22, 2025 2:34 AM UTC

Just curious what the filter is actually being used for - maybe there are alternative approaches that can be taken...

yonatan
yonatanAuthor
Associate III
May 25, 2025 2:33 PM UTC

I have to filter velocity derived by position[n] - position[n-1]

The sample freq is 50K and the cutoff should be less than 350 Hz