Question
Fluctuations on clkout pin under load
Posted on November 01, 2014 at 10:46
I've noticed that the output of the clkout pin is very near the frequency I would expect when a external crystal is used as the pll source, but fluctuates a little as the CPU performs gpio operations.
When I configure the internal oscillator as the PLL source, the frequency is a bit off, which I expected, but under loads it shows very large changes in frequency. Is this expected for the clock out behavior, or is this likely to be a power issue with my layout? Any suggestions on how to go about tracking down the cause, assuming its abnormal?