Skip to main content
James1
Associate II
October 23, 2018
Solved

Fluctuations in ADC value of STM32H743 MCU

Hi,

I have been working with STM ADC’s from quite a long time. I had used STM32F373 and F4 series MCU ADC’s earlier for my applications. As, now my application requires huge amount of RAM, memory and computation speed I have shifted to STM32H743 MCU . Earlier when I used F3 series ADC the noisy LSB was around 4 LSB which is a quite good resolution for 16 bit ADC . But as I have shifted to STM32H743 the noise level fluctuation is around 300LSB for 16 bit ADC resolution for single ended channel. When I hook up ground to ADC pin it shows a value fluctuation of about 100LSB . I use Analog accelerometer for my application and I need to see a resolution of 1 mg and with such amount of noise I won’t be able to achieve such high resolution.

The code is generated using CubeMx.The ADC is clocked using external clock and the MCU is powered from a 3.3 V regulator supply and Analog and digital grounds are properly separated.

I checked into their errata sheet and I couldn’t find any possible solution.

Any solutions will be highly appreciated .

Thank you

This topic has been closed for replies.
omuzychko
omuzychkoBest answer
Visitor II
October 11, 2019

PROBLEM SOLVED

Appears to be an issue of the Nucleo-144 demo-board itself (NUCLEO-H743ZI specifically), NOT AN STM32H7 FAULT!

HOW TO FIX?

  • Desolder/remove L2 ferrite bead to disable Ethernet PHY chip (see Nucleo-144 schematic, it is located close to that IC nearby Ethernet port).
  • Or use NUCLEO board without Ethernet hardware (OOOPS ... not available for H7)
  • Alternatively you may remove SB2, but that will disable USB-port circuitry as well

WHY?

  • This chip designated to PAM-modulate and amplify the Ethernet signal before feeding it into long wires of CAT5/6 cable.
  • Apparently it does not have any low-power/standby mode when not in use.
  • So even if you not use it - its clock (25MHz) injected into board circuitry (my guess - over the ground). Observed at ADC with 5mV peak-to-peak swing, basically reducing ADC resolution to 10-bits!

Can you have Ethernet and clean ADC capture at the same time?

  • Somewhat possible with oversampling or moving-average filter.
  • 16-samples needed to get 12 effective bits of resolution, but limits your acquisition bandwidth to around 100kHz

And here is my story of how did I figured it out:

First of all - sorry for a delay since my last reply. To approach this problem I had to wait for a good weekend (free of other tasks and events) since I decided to go "full ballistic" to eliminate any guess work:

  1. The Nucleo-144 board has been put into 3D-printed enclosure which was painted with MG Chemicals Super Shield conductive paint to block any external EMI sources.
  2. I've wired ADC inputs to 1.5V AAA battery. The wires were as short as I could get and battery did fit into shielded enclosure of the Nucleo board.
  3. I've used external power supply 8..12V.
  4. Also the ADC analog block (AVDD) was powered form the same LDO as the MCU itself. So MCU digital blocks can interfere with the ADC. It is always recommeded to use separate supply and even dedicated Vref for ADC. So I've soldered a separate circuit with 3.3V LDO isolated from the main external supply by capacitance multiplier (see EEVBolg youtube video on what is that: https://youtu.be/wopmEyZKnYo ).
  5. So SB12 (see Nucleo schematic) was de-soldered to connect this new clean-output LDO to AVDD. SBL162 was de-soldered as well and AGND was wired directly to the LDO ground pin. In other words AVDD and AGND of the nucleo board were now wired directly to its dedicated LDO.
  6. Test DC-signal source , the negative tab of 1.5V AAA battery was wired to the LDO ground. Eliminating ground loops for signal source.
  7. Add more bypass-capacitors for analog supply pins (soldered few more MLCCs on top of C34)

And then I've got the same high-speed (2 MSPS) raw data captures again:

0690X00000ApTaUQAV.png

as you see it still shows this aliasing affect, but it looks now way cleaner and more "pronounced" than it was before:

0690X00000AA9YCQA1.png

If using moving average filter using 2 samples, it improves slightly:

0690X00000ApTcVQAV.png

Trying to run ADC at its maximum sampling speed (5MSPS) did not help to figure out interference frequency, so it is higher than that.

As I've already mentioned in my previous post - you can not identify that this is aliasing of higher-frequency interference IF you do slow sampling. As in this 13kSPS example it just looks like Gaussian noise, because clock drift (PLL jitter) introduces a lot of phase noise to notice any aliasing patterns of 13kHz vs 25MHz interference.

0690X00000ARCUsQAP.png

For these who don't now:

ADC aliasing happens when there is higher frequency at your ADC input than the Nyquist frequency (more than 1/2 of you sampling speed). You can not work with this kind of acquired data if you want to do any decent signal processing on it. In all good designs ADC inputs are guarded with good low-pass filters. Here is good example from the web (https://e2e.ti.com/blogs_/archives/b/precisionhub/archive/2015/09/04/aliasing-in-adcs-not-all-signals-are-what-they-appear-to-be)

0690X00000ApTaeQAF.jpg

As you see 6 and 8 Hz signals can not be reproduced properly when sampling at 7Hz, you see that as 1Hz signal on ADC output.

In our case - the parasitic input was way beyond my Nyquist frequency of 1Mhz. If we zoom-in time scale of the first picture and plot it in MATLAB:

0690X00000ApTajQAF.png

The parasitic signal is apparently at 5mV peak to peak range (100 LSB out of 65536 for 3.3V full range).

Since all external sources were eliminated by shielding and ADC is powered by dedicated clean LDO there are few reasons left:

  • Internal issue in STM32H7 - highly unlikely. In datasheet we have SINAID specified at 82dB for single-ended input. If my calculations are correct - it should be equivalent of 5LSB RMS-noise. In other words - if measuring a perfect DC signal (from AAA-battery) 68% of samples should be with-in 10LSB range, and 99.7% for Gaussian noise should be with-in 30LSB peak-to-peak range.
  • Interfering signal source is some other component on the Nucleo-144 board, could be ST-Link as well getting something from USB-grouding.

To figure this out you need a spectrum analyser, LNA amplifier and H-field probe (https://youtu.be/crs_QLuUTyQ)

You can go cheaper way and get an SDR radio USB dongle with self-made H-field probe (https://www.stupid-projects.com/emc-probe-using-rtl-sdr)

I've found and ordered an MSi.SDR that has a perfect range for 10kHz to 2GHz for MCU board purposes.

Without having a patience to wait for SDR and semi-rigid coax delivery I've used an oscilloscope probe which came tip-to-BNC adapter. Using another female-to-feamale BNC-connector, piece of copper wire, aluminum foil and electric tape I've got an E/H-probe in like 20 min:

0690X00000ApTbcQAF.jpg0690X00000ApTbhQAF.jpg

With this contraption I was simply observing waveform on the scope and sniffed the interference source when I've stick it into Ethernet PHY IC package. I was lucky it was powerful enough to get me 5mV spikes on the scope without the need of any LNA.

Here is the raw sampling after I've thrown away an L2 ferrite bead. It should actually serve as a filter connecting a +3V3V_PER peripherals supply line to Ethernet PHY circuitry, but apparently interference is so strong that it propagates through the ground, or EMI into the wires connecting my DC-signal source to ADC input(s).

Here is the RAW capture of DC-signal source (AAA battery) after the hack:

0690X00000ApTc1QAF.png

And here its overlay (red) with the RAW capture before disabling Ethernet PHY (blue):

0690X00000ApTcGQAV.png

As you see - I've got it all well within spec, major half of samples are somewhat in 10LSB peak to peak range, while all of them within 30LSB.

26 replies

Khouloud GARSI
ST Employee
October 24, 2018

Hi @James​ ,

With the STM32F373 MCU, you were using an 12-bit ADC. Now with the STM32H743, you have a 16-bit one. Thus, it's normal that the noise level is more important using the STM32H7.

However, 100 LSB when the ADC is grounded stills a high value. 

Are you performing a SW ADC calibration? This is mandatory in in order to improve the conversion accuracy. If you're using ST drivers, this is done through function "HAL_ADCEx_Calibration_Start".

PS: You have highlighted that you have read the STM32H7 errata-sheet, please make sure that you're not facing one of the ADC limitations described there.

Khouloud

James1
James1Author
Associate II
October 25, 2018

Hi Khouloud,

Thank you very much for your reply. In STM32F373 MCU I was using 16 bit SDADC (Sigma Delta) and even for 16 bit ADC the noise was around 4 LSB.

But now when I compare the results of 12bit and 16bit ADC of STM32H743 it seems that there is just 4 bit amplification in the results.

I am using HAL libraries and even after doing calibration the results are similar no change. Now I seriously stuck with this noise problem.

James

Khouloud GARSI
ST Employee
November 2, 2018

Hi @James​ 

I advise you to have a look on the following recommendations and check if they are satisfied in your HW:

1) ADC voltage reference: Need low offset, low drift, and low-noise reference voltage.

2) Decoupling capacitors :

•  A pair of decoupling capacitor on Vref+ and on VDDA (1µFand 10nF) low inductive (0402 package recommended) ; should be placed very close to the MCU (especially the 10nF).

•  Each power supply pair should be decoupled with filtering ceramic capacitors (100 nF) and one single tantalum or ceramic capacitor (min. 4.7 μF) connected in parallel. These capacitors need to be placed as close as possible to, or below, the appropriate pins on the underside of the PCB.

3) PCB recommendation:

• Solid ground plane and PCB partitioned into analog and digital sections to prevent digital noise from interfering with analog sensitive signals.

4) ADC input Filter :

•  1 Capacitor to GND (47 pF recommended but value depends on application) to be placed very close to ADC input (will act as charge reservoir for current spikes when sampling switch is closed)

•  One resistor in series (value depends on application) in case filtering is needed.

Khouloud.

AvaTar
Senior III
October 24, 2018

> The ADC is clocked using external clock and the MCU is powered from a 3.3 V regulator supply and Analog and digital grounds are properly separated.

Have you checked the stability of VDDA ?

I would be wary of the high speed (= high power) characteristics of the H7, and consider an external ADC. Or an accelerometer with digital interface.

James1
James1Author
Associate II
October 25, 2018

Hi AVa Tar,

Thank you very much for your reply. I checked the stability of the power supply it is quite stable and even I have bypass capacitor banks on PCB and it’s a 4 layer PCB so the power supply should be good.

My application needs around 10K bandwidth and I couldn’t find any digital accelerometers with such high bandwidth so decided to use Analog accelerometer.

Ranjith

T J
Senior III
October 25, 2018

good project, I guess that you have a noise problem.. It is a custom board ?

they are quite specific about the 2.2uF Low ESR caps, did you use those ?

do you have SDRAM on your board ? ( very noisy)

can you supply the board from a battery not a switcher ?

Then you may see an improvement.

I would add more power supply filtering and ADC power filtering.

What impedance is the input drive ?

maybe you need to buffer the signal with an opamp

Edit:

Where did you join the Analog ground to the Digital ground ?

Martin Franke
Associate II
January 21, 2019

I don't know your setup, but quite a few limitation items exist on the STM32H743 errata sheet from ST: https://www.st.com/content/ccc/resource/technical/document/errata_sheet/group0/b8/f4/b7/a3/d1/a0/44/a6/DM00368411/files/DM00368411.pdf/jcr:content/translations/en.DM00368411.pdf

You might check the work-arounds listed. (This assumes you're using Revision Y silicon.)

MDief.15
Visitor II
June 7, 2019

Hi @James​ 

did you find a solution for the noise problem?

I have the same problem with the 16 bit ADC of the STM32H7: 300 - 350 LSBs of noise on my signal.

I also used the ADCs of the STM32F3 and F4 in the past an had no issues there.

With the STM32H7 I see the noise on my custom board and also on the NUCLEO-H743ZI Board.

On the nucleo board I tied a 22k/10k voltage divider from 3V3 to PA6 and measured it with ADC1. I also added 100 nF for filtering.

The values which I get from the ADC vary between 20333 and 20682.

Matthias

omuzychko
Visitor II
August 22, 2019

Last few weeks I've been evaluating Nucleo-144 board with STM32H743ZI. Experiencing similar issue I would like to share my findings here.

According to spec for single-ended Rev Y (400Mhz) the given EOB/SNR/SINAID in ideal scenario we should result int noise fluctuations of around 16LSB (maybe higher occasional peak-to-peak values, but majority of samples should stay in this range), not 200..300 as reported.

So far I think Nucleo-144 H743ZI board does not have sufficient decoupling for AVDD and Vref pins, high-frequency noise is injected into conversion which produces aliasing errors, making some DSP post-processing in my application quite inaccurate. The ADC itself, when turns ON creates fluctuations on AVDD line, that loops back over Vref.

So, I am sampling 4 channels with 2 ADCs, where each ADC scans through two assigned channels (2.6 MHz, so 1.3MHz sampling rate per channel).

I am have configured DMA with double-buffering to eventually run DSP processing in background, without the need to ever stop ADC acquisition.

On the oscilloscope images:

  • Yellow channel is AVDD (AC-coupled) where scope probe is hooked to AVDD and AGND pinheaders of the Nucleo 144.
  • Pink channel is an onboard blue LED, which goes down when ADC acquisition starts and goes up when DMA half-transfer complete. So main thread begins processing of first half-buffer, while second half-buffer acquisition still in progress. Half buffer length 1728 samples (full buffer is 3456). Since ADC multiplaxes between two channels - there are total 6912 samples acquired.

So to troubleshoot the problem first thing is to figure out and mitigate all the contributing noise sources.

External battery supply with NO USB connected,:

0690X00000AA9VcQAL.png

Here how noisier it becomes with connected USB ground:

0690X00000AA9W1QAL.png

And here is the same (with battery power and connected USB) with added electrolytic capacitor on AVDD and AGND pin.

A miserable attempt to improve analog supply decoupling, looks slightly cleaner. But with grain of salt - cap inserted on the line between MCU pins and scope input, so it could be just "LPF-ing" the signal which goes into oscilloscope probe, while the analog supply itself is still noisy:

0690X00000AA9VwQAL.png

Here is AVDD line with slighly better zoom in time domain:

0690X00000AA9WVQA1.png

Attention - my scope is 100MHz bandwidth, so what you see might be aliasing of much higher frequencies.

Anyway 5 mV p-p fluctuation is likely contributes to sampled values accordingly.

With 3.3V supply on Vref a 5mV noise will result into 2.5mV error of measured signal that is half of sumplu line (1.6V) and that is eqvivalent of ~100LSB. Moreover - for a signal that is closer to 3.3V supply line it will increase to 200LSB.

On next scope screenshot the new blue channel is hooked up to one of the ADC channels (pin-header of the Nucleo board). For an experiment I've disconnected the analog circuitry of my sensor and dropped in a pre-charged capacitor. So I get a steady fixed DC input into ADC:

0690X00000AA9XxQAL.png

These spikes on the channel line are actual moments when ADC performs "sampling" phase in its "sample and hold" circuitry (latching to charge an internal capacitor).

This seem to be in-sync with fluctuations on AVDD line (yellow). But you see that AVDD level fluctuation is double the frequency than spikes on the ADC channel line - that is because I have an ADC module configured to multiplex between two input channels. So AVDD level sags whenever actual ADC conversion is in progress.

Here is actual sampled data on a channel (orange dots - actual samples, blue line - is a spline interpolation):

0690X00000AA9YCQA1.png

  

It looks like aliasing with higher frequency interference (sampling here is 1.333 Mhz per channel, accordingly ADC triggered at double of that - 2.666Mhz).

You got to be careful when trying to get measurements like this. Here how it looks when I am holding with my fingers the insulated wires to the capacitor that is being measured:

0690X00000AA9YRQA1.png

Next steps are:

  • Try dedicated supply LDO for AVDD/VRef.
  • EMI shielding (I have it all assembled in the 3D printed enclosure which I will try paint with MG Chem Super Shield). This will not save me from internal EMI emissions by STM32H7 itself.
  • Y to V revision update brings some good improvements. Errata doc mentions some problems with simultaneous ADC conversation - I did not check that yet (had two ADC modules sampling simultaneously during all experiments above)
  • I am committed to nail it down and get the spec-ed performance. But a bit worried for BGA100 package that I was planning to use in final 4-layer board design. It does NOT have Vref input which is my current suspect of all problems! Only AVDD pin which has Vref hooked up internally, so heavy simultaneous use of analog circuitry may deteriorate sampling.

SF??r
Associate III
September 13, 2019

We had also some issues to avoid ADC "glitches" up to 2000 digits at 16 Bit mode...

Disabling the DAC solve this problem (disable the DAC buffer reduce the problem). The DAC brings strange voltage spikes to VRef+.... I don't know why, because the driving voltage should be AVCC not VRef+.

Singh.Harjit
Senior
September 13, 2019

Wonderful analysis! I don't have experience with the STM32H743 yet but consider adding the following to your next steps:

1) Stop the processor during the ADC conversion - do a WFI() and see if that helps. If this helps, then, it is on chip or board noise coupling.

2) What is the source impedance of the channel? I would try adding an Op-Amp (temporarily) to see if that helps

3) Another thing to try is to do these measurements while sweeping the sampling time from min to max. If this affects things, then, it points to a source impedance / STM32H7 ADC input circuit interaction.

omuzychko
Visitor II
September 13, 2019

Here 2x ADC modules with 2 channles per each during simultaneous sampling each pair of channels at much lower frequecy (~13 kSPS)0690X00000ARCUsQAP.png

Basically - the range of min-max values are are the same, as at the high frequency. But you can't not see that there is some aliasing happening because sampling speed is slower by a factor of hundreds. So the noise looks completely random.

I do have a unity-gain buffer on each channel between my sensor circuitry and ADC inputs of STM32H7. In fact for the purity of tests I've connected the ADC input to a AA battery. Also if trying to measure DC level (like a battery voltage) - the source impedance might not need to be very low, since sample and hold capacitor stays charged at the same level between samples.

I've came to understanding that the ripple I see on AVdd is exactly double of sampling frequency. Because I actually have 2 channels enabled per ADC module in scan mode. The sampling is triggered by timer that runs twice faster than the needed sampling frequency per single channel. So the observed ripple appears to be the sag of supply voltage when ADC preforms sample conversion on each channel. So there is no guarantee it restores to exactly the same level before S/H on the next channel, and that is actually expected to produce such aliasing-like strange effects (assuming if the level of AVdd sag is dependent on the actual converted value).

I still have to run the testing with proper dedicated AVdd supply. The ferrite bead installed on Nucleo boar may represent high AVdd supply impedance when sampling frequency is very high. Also if it sags during conversion itself - than the Vref is changing as well while converting each subsequent bit.

Accordingly the actual ADC clock may play a major role here as well. Clocking ADC slower should make AVdd sag during conversion less steep or non existent at all (just some spikes on each bit conversion). What I am trying to say is that changing the clock of sampling timer (that triggers my ADC module) probably did not help because ADC was still running at a very high clock rate. I had to reduce the ADC clock frequency to the minimum as well, so the expectation will be less diturbance on AVdd and more pure conversion result.

All these "reduce speed" tricks however won't work for my application because I need high sampling speeds (at least 2MSPS per channel for 4 channels).

Singh.Harjit
Senior
September 25, 2019

Any updates / progress on reducing the noise on the STM32H743 ADC?

omuzychko
omuzychkoBest answer
Visitor II
October 11, 2019

PROBLEM SOLVED

Appears to be an issue of the Nucleo-144 demo-board itself (NUCLEO-H743ZI specifically), NOT AN STM32H7 FAULT!

HOW TO FIX?

  • Desolder/remove L2 ferrite bead to disable Ethernet PHY chip (see Nucleo-144 schematic, it is located close to that IC nearby Ethernet port).
  • Or use NUCLEO board without Ethernet hardware (OOOPS ... not available for H7)
  • Alternatively you may remove SB2, but that will disable USB-port circuitry as well

WHY?

  • This chip designated to PAM-modulate and amplify the Ethernet signal before feeding it into long wires of CAT5/6 cable.
  • Apparently it does not have any low-power/standby mode when not in use.
  • So even if you not use it - its clock (25MHz) injected into board circuitry (my guess - over the ground). Observed at ADC with 5mV peak-to-peak swing, basically reducing ADC resolution to 10-bits!

Can you have Ethernet and clean ADC capture at the same time?

  • Somewhat possible with oversampling or moving-average filter.
  • 16-samples needed to get 12 effective bits of resolution, but limits your acquisition bandwidth to around 100kHz

And here is my story of how did I figured it out:

First of all - sorry for a delay since my last reply. To approach this problem I had to wait for a good weekend (free of other tasks and events) since I decided to go "full ballistic" to eliminate any guess work:

  1. The Nucleo-144 board has been put into 3D-printed enclosure which was painted with MG Chemicals Super Shield conductive paint to block any external EMI sources.
  2. I've wired ADC inputs to 1.5V AAA battery. The wires were as short as I could get and battery did fit into shielded enclosure of the Nucleo board.
  3. I've used external power supply 8..12V.
  4. Also the ADC analog block (AVDD) was powered form the same LDO as the MCU itself. So MCU digital blocks can interfere with the ADC. It is always recommeded to use separate supply and even dedicated Vref for ADC. So I've soldered a separate circuit with 3.3V LDO isolated from the main external supply by capacitance multiplier (see EEVBolg youtube video on what is that: https://youtu.be/wopmEyZKnYo ).
  5. So SB12 (see Nucleo schematic) was de-soldered to connect this new clean-output LDO to AVDD. SBL162 was de-soldered as well and AGND was wired directly to the LDO ground pin. In other words AVDD and AGND of the nucleo board were now wired directly to its dedicated LDO.
  6. Test DC-signal source , the negative tab of 1.5V AAA battery was wired to the LDO ground. Eliminating ground loops for signal source.
  7. Add more bypass-capacitors for analog supply pins (soldered few more MLCCs on top of C34)

And then I've got the same high-speed (2 MSPS) raw data captures again:

0690X00000ApTaUQAV.png

as you see it still shows this aliasing affect, but it looks now way cleaner and more "pronounced" than it was before:

0690X00000AA9YCQA1.png

If using moving average filter using 2 samples, it improves slightly:

0690X00000ApTcVQAV.png

Trying to run ADC at its maximum sampling speed (5MSPS) did not help to figure out interference frequency, so it is higher than that.

As I've already mentioned in my previous post - you can not identify that this is aliasing of higher-frequency interference IF you do slow sampling. As in this 13kSPS example it just looks like Gaussian noise, because clock drift (PLL jitter) introduces a lot of phase noise to notice any aliasing patterns of 13kHz vs 25MHz interference.

0690X00000ARCUsQAP.png

For these who don't now:

ADC aliasing happens when there is higher frequency at your ADC input than the Nyquist frequency (more than 1/2 of you sampling speed). You can not work with this kind of acquired data if you want to do any decent signal processing on it. In all good designs ADC inputs are guarded with good low-pass filters. Here is good example from the web (https://e2e.ti.com/blogs_/archives/b/precisionhub/archive/2015/09/04/aliasing-in-adcs-not-all-signals-are-what-they-appear-to-be)

0690X00000ApTaeQAF.jpg

As you see 6 and 8 Hz signals can not be reproduced properly when sampling at 7Hz, you see that as 1Hz signal on ADC output.

In our case - the parasitic input was way beyond my Nyquist frequency of 1Mhz. If we zoom-in time scale of the first picture and plot it in MATLAB:

0690X00000ApTajQAF.png

The parasitic signal is apparently at 5mV peak to peak range (100 LSB out of 65536 for 3.3V full range).

Since all external sources were eliminated by shielding and ADC is powered by dedicated clean LDO there are few reasons left:

  • Internal issue in STM32H7 - highly unlikely. In datasheet we have SINAID specified at 82dB for single-ended input. If my calculations are correct - it should be equivalent of 5LSB RMS-noise. In other words - if measuring a perfect DC signal (from AAA-battery) 68% of samples should be with-in 10LSB range, and 99.7% for Gaussian noise should be with-in 30LSB peak-to-peak range.
  • Interfering signal source is some other component on the Nucleo-144 board, could be ST-Link as well getting something from USB-grouding.

To figure this out you need a spectrum analyser, LNA amplifier and H-field probe (https://youtu.be/crs_QLuUTyQ)

You can go cheaper way and get an SDR radio USB dongle with self-made H-field probe (https://www.stupid-projects.com/emc-probe-using-rtl-sdr)

I've found and ordered an MSi.SDR that has a perfect range for 10kHz to 2GHz for MCU board purposes.

Without having a patience to wait for SDR and semi-rigid coax delivery I've used an oscilloscope probe which came tip-to-BNC adapter. Using another female-to-feamale BNC-connector, piece of copper wire, aluminum foil and electric tape I've got an E/H-probe in like 20 min:

0690X00000ApTbcQAF.jpg0690X00000ApTbhQAF.jpg

With this contraption I was simply observing waveform on the scope and sniffed the interference source when I've stick it into Ethernet PHY IC package. I was lucky it was powerful enough to get me 5mV spikes on the scope without the need of any LNA.

Here is the raw sampling after I've thrown away an L2 ferrite bead. It should actually serve as a filter connecting a +3V3V_PER peripherals supply line to Ethernet PHY circuitry, but apparently interference is so strong that it propagates through the ground, or EMI into the wires connecting my DC-signal source to ADC input(s).

Here is the RAW capture of DC-signal source (AAA battery) after the hack:

0690X00000ApTc1QAF.png

And here its overlay (red) with the RAW capture before disabling Ethernet PHY (blue):

0690X00000ApTcGQAV.png

As you see - I've got it all well within spec, major half of samples are somewhat in 10LSB peak to peak range, while all of them within 30LSB.