Skip to main content
Channamallesh Hiremath
Associate II
May 3, 2018 9:36 PM UTC
Question

flashing stm32F303 based custom board

Posted on May 03, 2018 at 23:36

Hello,

I am making a custom board based on STM32F3 discovery board. My custom board is an exact copy of the discovery board with additional sensor components. 

I can easily program STM32F3 board as st-link is already built on to the board. 

How do I do the same thing when I get my boards done?

I do have both 

STM32F103C8T6

  processor and 

STM32F303VCT6

 on the system.

Is there a code for 

STM32F103C8T6 which I can use to flash the board? 

Can you please help me with this?

Best Regards,

Mallesh 

    This topic has been closed for replies.