Question
Flash write on STM32L431RCt6
Hi there,
I have a STM32L431RCT6 microcontroller. I wish to write some data on it. let's say I want to write 2 at 0x08009000 Address.
here is my code
#define FLASH_USER_START_ADDR ((uint32_t)0x08009000)
#define FLASH_USER_END_ADDR ((uint32_t)0x08009000) + FLASH_PAGE_SIZE
#define DATA_SIZE 2and here is the code where I call flash wirte
flash_buffer_w[1]=2;
write_data_to_flash(flash_buffer_w,DATA_SIZE);and here is the definition of write_data_to_flash()
uint8_t write_data_to_flash(int32_t *data,uint16_t size)
{
uint32_t NbOfPages = 0;
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Clear OPTVERR bit set on virgin samples */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* Unlock the Options Bytes *************************************************/
HAL_FLASH_OB_Unlock();
/* Get the number of the start and end pages */
StartPage = GetPage(FLASH_USER_START_ADDR);
EndPage = GetPage(FLASH_USER_END_ADDR);
/* Get the number of pages to erase from 1st page */
NbOfPages = GetPage(FLASH_USER_END_ADDR) - StartPage + 1;
/* Erase the user Flash area
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.Page = FLASH_USER_START_ADDR;
EraseInitStruct.NbPages = NbOfPages;
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
{
/*
Error occurred while page erase.
User can add here some code to deal with this error.
PAGEError will contain the faulty page and then to know the code error on this page,
user can call function 'HAL_FLASH_GetError()'
*/
a1=-1;
}
/* Program the user Flash area word by word
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
Address = FLASH_USER_START_ADDR;
for(uint32_t i=0;i<size;i++)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, flash_buffer_w[i]) == HAL_OK)
{
Address = Address + 8;
}
else
{
/* Error occurred while writing data in Flash memory.
User can add here some code to deal with this error */
a1=-2;
}
}
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
}but what happens is that the erasing process happens in a way that it even erases some pages form the very beginning Address of the whole program i.e. Address 0x8000000!!!
why this happens?
any solution?