Skip to main content
Arlet Ottens
Associate II
June 1, 2020
Question

Flash read through debugger not working when using WFE/WFI

  • June 1, 2020
  • 0 replies
  • 552 views

I am using an STM32F429VGT6 with SWD debugger, and OpenOCD software 0.10.0.

I am trying to dump the contents of the flash memory at 0x08000000.

If I don't use any WFE/WFI in my code, this works fine.

If I put a WFE at the beginning of the code, before any interrupts are enabled, the device is in continuous SLEEP mode, and I also have no problems reading the flash memory.

However, when I used WFE in normal code, and the device is switching between run/sleep modes, I sometimes get the wrong output when dumping the flash. There are no errors reported, but it just shows the wrong data.

In all cases, the debugger sets DBGMCU_CR to 7. I am not using STOP/STANDBY mode, just sleep.

I have also tried this on a STM32F427VIT6, and everything works fine there.

This topic has been closed for replies.