Skip to main content
CDan.1
Associate II
Nov 17, 2022 1:05 PM UTC
Solved

Flash Programming Error Even if Flash was erased.

Hi guys,

I am using and STM32L552ZET6 and I get a behavior I can not exaplain. The device is power at 1.8V in case it matters. So to put it shortly I have 2 blocks of 8 pages each. At first start I erase both of the blocks and write only in block 1 some data. When I get some data to save I write it in block 2 but first I write two doublewords used as markers on top of the first page of block 2 after which I copy most of the data from the first block. My problem is that for the first 24 octets I try to write I get back NSPROGERR and NSPGSERR, and for the rest everything works out great and are written.

If I erase the page again just before writeing I get no errors and everything gose perfect.

I have tried to debug it by printing the info found in the locations just before programming and I get 0xFFFFFFFFFFFFFFFF in each location with problems.

This is the function I use to program:

static void FLASH_Program_DoubleWord(uint32_t Address, uint64_t Data)

{

 uint32_t primask_bit;

 __IO uint32_t *reg;

 /* Check the parameters */

 assert_param(IS_FLASH_PROGRAM_ADDRESS(Address));

 /* Access to SECCR or NSCR registers depends on operation type */

 reg = IS_FLASH_SECURE_OPERATION() ? &(FLASH->SECCR) : &(FLASH_NS->NSCR);

   if((Address>=0x08078000 && Address<(0x08078000 +0x0018)) ||(Address>=0x0807C000 && Address<(0x0807C000 +0x0018)))

   {

 uint8_t c[10];

 hex2str(*(uint32_t*)Address,c,4);

 USART_AddBuffer(2, c,10, 1);

 hex2str(*(uint32_t*)(Address+4U),c,4);

 USART_AddBuffer(2, c,10, 1);

 USART_TransmitBuffers(2);

   }

 /* Disable interrupts to avoid any interruption during the double word programming */

 primask_bit = __get_PRIMASK();

 __disable_irq();

 /* Set PG bit */

 SET_BIT((*reg), FLASH_NSCR_NSPG);

 /* Program first word */

 *(uint32_t*)Address = (uint32_t)Data;

 /* Barrier to ensure programming is performed in 2 steps, in right order

   (independently of compiler optimization behavior) */

 __ISB();

 /* Program second word */

 *(uint32_t*)(Address+4U) = (uint32_t)(Data >> 32U);

 /* Re-enable the interrupts */

 __set_PRIMASK(primask_bit);

}

This function is called from this function:

uint8_t FLASH_Program(uint32_t TypeProgram, uint32_t Address, uint64_t Data)

{

 uint8_t status=FLASH_OK;

 __IO uint32_t *reg;

 /* Wait for last operation to be completed */

 status = FLASH_WaitForLastOperation(FLASH_TIMEOUT_VALUE);

 if(status == FLASH_OK)

 {

   pFlash.ProcedureOnGoing = TypeProgram;

   reg = IS_FLASH_SECURE_OPERATION() ? &(FLASH->SECCR) : &(FLASH_NS->NSCR);

   /* Program double-word (64-bit) at a specified address */

   FLASH_Program_DoubleWord(Address, Data);

   /* Wait for last operation to be completed */

   status = FLASH_WaitForLastOperation(FLASH_TIMEOUT_VALUE);

   /* If the program operation is completed, disable the PG Bit */

   CLEAR_BIT((*reg), (pFlash.ProcedureOnGoing & ~(FLASH_NON_SECURE_MASK)));

 }

 else

 {

   status=FLASH_LAST_OP;

 }

 /* Process Unlocked */

 return status;

}

Mainly the ideea is I get the NSPGSERR and NSPROGERR even if on the locations I want to write is 0xFFFFFFFFFFFFFFFF. I have checked this by reading before writing and also using STMProgrammer.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Nov 17, 2022 1:33 PM UTC

Error code correction (ECC) Dual bank mode (DBANK=1, 64-bits data width) Data in Flash memory are 72-bits words: 8 bits are added per double word (64 bits). The ECC mechanism supports: • One error detection and correction per 64 double words • Two errors detection

You cant prog twice irelevant FFF

3 replies

MM..1
MM..1Best answer
Super User
Nov 17, 2022 1:33 PM UTC

Error code correction (ECC) Dual bank mode (DBANK=1, 64-bits data width) Data in Flash memory are 72-bits words: 8 bits are added per double word (64 bits). The ECC mechanism supports: • One error detection and correction per 64 double words • Two errors detection

You cant prog twice irelevant FFF

CDan.1
CDan.1Author
Associate II
Nov 17, 2022 2:39 PM UTC

Regarding ECC I do not use it, but this part "You cant prog twice irelevant FFF" made me realise somthing......when I program the controller first time I write that page with FFFF....

MM..1
Super User
Nov 17, 2022 2:44 PM UTC

You cant dont use ECC, is by design on FLASH, read reference manual about internal flash.