Skip to main content
Moritz Diller
Associate III
Jul 8, 2018 10:58 AM UTC
Solved

Flash programming alignment error, STM32L433CC, TrueStudio

Posted on July 08, 2018 at 12:58

I'm trying to debug a project in TrueStudio, but get this error message during flashing:

0690X0000060LgyQAE.png

... which is the ''load'' instruction of the startup script.

I think the cause of this error is, that the flash size of my program can't be divided by 4 without remainder:

Print size information

text          data    bss       dec          hex

132474    640    38232    171346    29d52

If I modify the project by inserting a while(1) before the use of the library, which makes the flash size not a multiple of 4 bytes, it can be flashed.

Console output:

Flash write: Address= 0x800d0a8, Length=70

Programming flash..

STM32 device: flash programming successful 0x800d0a8

Flash write completed in 0.085000 seconds, 0.804228kB/s

Flash write: Address= 0x800d0ee, Length=126

Programming flash..

Flash programming alignment error

I ported this project from an F3 MCU to the L4 MCU. The F3 project could be flashed by TrueStudio without any problem and had a flash size which was not a multiple of 4 bytes, too.

I can program the hex-file with ST-Link-Utility and debug with TrueStudio by removing the load-instruction from the startup file, but of course that's not convenient.

    This topic has been closed for replies.
    Wellington Santos
    Visitor II
    Oct 31, 2018 9:15 PM UTC

    I had the same problem.

    Update to the new Atollic version 9.1.0. This solved the question to me.

    2 replies

    Tesla DeLorean
    Guru
    Aug 10, 2018 4:27 AM UTC

    @AtollicSupport

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Wellington Santos
    Visitor II
    Oct 31, 2018 9:15 PM UTC

    I had the same problem.

    Update to the new Atollic version 9.1.0. This solved the question to me.