Skip to main content
Associate II
November 28, 2023
Solved

flash memory write problem

hello experts ,my device is stm32f103c8t6 ,cubeide 1.14.0

it shows 64kb flash in ide but shows 128kb in stmcube programmer ,my issue is if i write flash from inside the programme while mcu running then it writes fine but when i erase the page and try to write again it does not write , my code is here ,

HAL_FLASH_Unlock();

HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, 0x0800FC00,1000);// page 63

//write fine until here

HAL_Delay(100);

FLASH_PageErase(0x0800FC00); //page 63

//erase page ok but after using erase it doesnt wite anything

HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, 0x0800FC04,1000);//defaults

HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, 0x0800FC06,100);//d

do anyone know problem ?

i am trying to use a memory page as eeprom

This topic has been closed for replies.
ahmashBest answer
Associate II
November 28, 2023

I used this method and it worked thanks everyone

erasePage63();

// Function to erase page number 63

void erasePage63(void) {

FLASH_EraseInitTypeDef eraseInitStruct;

uint32_t pageError = 0;

 

// Erase settings

eraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; // Erase type: Page erase

// 0x08000000 + (63 * 1024) = 0x0800FC00 //63 is page no and you can use different

eraseInitStruct.PageAddress = 0x0801FC00; // Start address of page 63

eraseInitStruct.NbPages = 1; // Number of pages to erase

 

// Erase page

HAL_FLASHEx_Erase(&eraseInitStruct, &pageError);

 

if (pageError != 0) {

// An error occurred during erasing

// Handle the error here

}

}

3 replies

ST Employee
November 28, 2023

Hello @ahmash 

Try to read out the PER bit value of the FLASH_CR register after the erase. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
November 28, 2023

> FLASH_PageErase(0x0800FC00); //page 63

To erase a page, call HAL_FLASHEx_Erase, not FLASH_PageErase.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ahmashAuthorBest answer
Associate II
November 28, 2023

I used this method and it worked thanks everyone

erasePage63();

// Function to erase page number 63

void erasePage63(void) {

FLASH_EraseInitTypeDef eraseInitStruct;

uint32_t pageError = 0;

 

// Erase settings

eraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; // Erase type: Page erase

// 0x08000000 + (63 * 1024) = 0x0800FC00 //63 is page no and you can use different

eraseInitStruct.PageAddress = 0x0801FC00; // Start address of page 63

eraseInitStruct.NbPages = 1; // Number of pages to erase

 

// Erase page

HAL_FLASHEx_Erase(&eraseInitStruct, &pageError);

 

if (pageError != 0) {

// An error occurred during erasing

// Handle the error here

}

}