Skip to main content
Visitor II
May 2, 2024 8:45 AM UTC
Question

Flash Memory

We are using STM32F373VCT6 Microcontroller for our application and we want to use an External Flash Memory of 1MB with this controller. Can you suggest some NAND/NOR Flash memory of 1MB, that supports SPI/QSPI and is compatible with this controller and driver IC's.

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
May 2, 2024 9:41 AM UTC

STM32F37x has no memory mappable interface for external flash/ram. Either go to a family with such interface or use flash on SPI and load from spi to ram on demand.

Tesla DeLorean
Guru
May 2, 2024 10:46 AM UTC

You could wire a small Winbond W25Q SPI NOR Flash device

You could use a SOIC8 or SOIC16W foot print or dual one allowing either, to provide many options for.part choice. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..