Skip to main content
bngstskn
Associate III
September 28, 2023
Solved

FLASH Mem Error

I use an STM32F030F4 chip. The code I wrote is quite short. But when I compile I get this error. And STM32F0 has 16 to 256 Kbytes of Flash memory. I don't understand why it is an error. Does anyone know why?

 

c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: STM32F0.elf section `.text' will not fit in region `FLASH'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: region `FLASH' overflowed by 952 byte
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC_Init();
 MX_I2C1_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 if (HAL_ADC_Start(&hadc) != HAL_OK)
	 {
	 Error_Handler();
	 }

	 // ADC dönüşümünün tamamlanmasını bekle
	 if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) != HAL_OK)
	 {
	 Error_Handler();
	 }

	 // ADC değerini oku
	 uint16_t adcValue = HAL_ADC_GetValue(&hadc);

	 // ADC değerini sıcaklık değerine çevirin
	 float resistance, temperature;
	 resistance = 100000.0 / ((4095.0 / adcValue) - 1.0);
	 temperature = (1.0 / ((log(resistance / 100000.0) / 3950.0) + (1.0 / 298.15))) - 273.15;

	 // Dönüşüm sonuçlarını kullanın veya görüntüleyin
	 // temperature, sıcaklık değerini içerir

	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}

 

 

This topic has been closed for replies.
TDK
TDKBest answer
September 28, 2023

> region `FLASH' overflowed by 952 byte

As the error message says, your code is too large for the flash you have available. Your chip only has 16 kB of FLASH, which is not much.

You can reduce the size of the code by changing optimization settings from Debug to Release.

Also, in particular, using doubles is increasing your code size a lot. Put "f" at the end of a number to make it a float instead. For example, use "1.0f" instead of "1.0". Your chip doesn't have an FPU so using floating point at all will increase size a fair amount. Sticking to integers would help with this.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
September 28, 2023

> region `FLASH' overflowed by 952 byte

As the error message says, your code is too large for the flash you have available. Your chip only has 16 kB of FLASH, which is not much.

You can reduce the size of the code by changing optimization settings from Debug to Release.

Also, in particular, using doubles is increasing your code size a lot. Put "f" at the end of a number to make it a float instead. For example, use "1.0f" instead of "1.0". Your chip doesn't have an FPU so using floating point at all will increase size a fair amount. Sticking to integers would help with this.

"If you feel a post has answered your question, please click ""Accept as Solution""."
bngstskn
bngstsknAuthor
Associate III
September 28, 2023

this was bad. Then would it be better if I use STM32F030RCT6? I need to use a very cheap chip. Do you have any suggestions on this matter?

TDK
September 28, 2023

I listed some suggestions above. I would suggest looking at those.

As for finding cheap chips, I would look at STM32 chips and sort by price and choose the cheapest one that fit my needs.

"If you feel a post has answered your question, please click ""Accept as Solution""."