Skip to main content
RLalj.1
Associate II
October 22, 2020
Question

Flash download error: Failed to open .sim file| IAR Workbench

  • October 22, 2020
  • 3 replies
  • 3983 views

Hello Everyone,

I'm using STM32H7 family microcontroller and when try to debug the code from IAR Workbench there is a error popup on my screen like " Flash download error: Failed to open file 'Project Folder\EWARM\Project\Exe\ProjectName.sim' ". After several try (almost 5-7 or sometime more than 10) it works, debug code working fine. So I think it couldn't get this sim file properly.

0693W000005918xQAA.jpg 

Simple Code (.sim) file is generated by debugger at the time of debug.

This process becomes time consuming for me every time I debug the code. I tried google search but there is no article or discussion about this type of problem.it may be bug or configuration issue in IAR workbench.

Has anyone been got these type of error before ? Please share your suggestions and solution for this problem.

Thanks in advance.

Note : IAR Workbench V8.40.1, ST-Link V2

Incl: Attached error message ss from IAR workbench.

This topic has been closed for replies.

3 replies

MMostafa
Associate II
October 27, 2020

I suddenly have the same issue exactly, but it never works now even after 10 trails. If you found a solution, please share it.

ssooki
Associate III
April 1, 2021

I suffered from the same symptoms for a while.

After deleting the sim file and rebuilding, no error message appeared and it worked normally.

RLalj.1
RLalj.1Author
Associate II
April 6, 2021

Yeah, that's the only solution to this problem. Try a different version of IAR that might resolve the problem.