Skip to main content
rasyoung
Associate
December 12, 2010
Question

Fix for gdbserver not starting TrueStudio Lite ...

  • December 12, 2010
  • 1 reply
  • 629 views
Posted on December 12, 2010 at 21:32

See following discussion:

Sirs,

Thanks for the consideration of your reply. Yes I am aware of the ''SWD'' issue, but I

think what worked for me was flashing the St-link to the LATEST version of the firmware

distributed in TrueStudio Lite 1.4. Now it is working!

Lots to learn here. The instructions on how to use the firmware samples from ST (an3268)

with you product are very POOR. Not your fault, unclear in the downloaded zip file

instructions... I can compile but not link.

Much to learn!

Thanks again.

Randy

ps. Yes gdbserver runs on Windows 64~!

Quoting Atollic support <>:

https://webmail.iu.edu/horde/imp/message.php?index=14194#

Dear Randy,

Which board are you using?

If you are using the STM32 Discovery board - One reason could be if

it is a Discovery board you need to connect using SWD mode.

If you create a new project with the TrueSTUDIO wizard for the

Discovery board it will create a project that make some LED toggling

for the board. When starting first debug session TrueSTUDIO

ST has had a problem with the sw they have on the web for the

Discovery board. It shall be fixed now so that it contain correct

debug setting with SWD mode also for TrueSTUDIO. Try to download the

sw again from ST web site.

Please let me know if this helps.

Best regards,

Atollic support

&nbsp;

On  09/12/2010, 23:42, ''Young,  Randall Shane'' () wrote:

Sirs,

On windows 64. ST-Link device not found. Yes I have followed

instructions exactly as to connect ST-Link and hardware, power, usb,

etc. as posted on your web page. IAR eW5 works perfectly with ST-Link...

Suggestions?

Randy

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    December 14, 2010
    Posted on December 14, 2010 at 05:51

    Well it really is Atollic's fault that the evaluation features of Lite make it next to unusable.

    It's easy for them to blame ST, but it's an up hill battle to get their tool chain to build, link and download a simple project. I've done it, but had to waste a lot of time.

    The demo projects provide by ST had to be generated by a NON LITE version, it's not ST's fault that it's such a total train wreck. Sure there's some blame, but most of that's because the project, path and directory setting don't map well to the flexible placement of the project on a disc. The problem is compounded by the fact that it is very difficult to modify paths/files in the project to correct issues where it can't find files.

    Seriously, try the eval versions of KEIL and IAR

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..