Skip to main content
cyril2399
Associate III
Jul 11, 2011 7:28 AM UTC
Question

first program of stm3210C

Posted on July 11, 2011 at 09:28

Hello,

I have a stm3210C eval board and when I have launched it there was a program with sound, image, a game, web server all with icons.

I have download an example program and now I it is the only thing I have on my eval board.

I would like to found the first program that it had at the beginning.

Where could I find it ?

Thanks
    This topic has been closed for replies.

    7 replies

    rosarium
    Associate
    Jul 11, 2011 7:40 AM UTC
    Posted on July 11, 2011 at 09:40

    STM3210C-EVAL demonstration firmware  at

    http://mcd.rou.st.com/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware

    rosarium
    Associate
    Jul 11, 2011 7:44 AM UTC
    cyril2399
    cyril2399Author
    Associate III
    Jul 12, 2011 7:19 AM UTC
    Posted on July 12, 2011 at 09:19

    ok thank you very much, I've found what I need. Thanks

    rosarium
    Associate
    Jul 12, 2011 8:21 AM UTC
    Posted on July 12, 2011 at 10:21

    You are welcome... :)

    cyril2399
    cyril2399Author
    Associate III
    Jul 18, 2011 7:39 AM UTC
    Posted on July 18, 2011 at 09:39

    Hello,

    Into the firmware, the project ''DEMO'' has an empty main...

    the whole program is ''int main() {}''.

    I would like to see how it is programmed (icons, image player, system info etc...).

    Thank you

    cyril2399
    cyril2399Author
    Associate III
    Aug 24, 2011 1:04 PM UTC
    Posted on August 24, 2011 at 15:04

    Is there no way to have these codes?

    Tesla DeLorean
    Guru
    Aug 24, 2011 3:42 PM UTC
    Posted on August 24, 2011 at 17:42

    Is there no way to have these codes?

    It is no doubt using commercially licensed libraries, and you'd have to pay for them yourself.

    You should probably contact ST, or your FAE, to discuss the availability of source code, or portions thereof. I suspect supporting the application for everyone would tax the engineering resources available.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..