Question
First boot on new target board
Posted on June 19, 2013 at 18:30
Powered up newly designed board today.
Of course it seems not to work. :( Its based on Discovery board. I currently have only the STM portion populated. The Oscillator pins are both low. Using a 8 Mhz Xtal and 20 pf caps. I would of expected one high one low and oscillating. Part is STM32F407VGT6 100QFP I seems to have 3.3V and 1.8 on P73 and P49 Reset goes both low and high with reset switch. Seems to draw 7.5ma. Anyone got a checklist to go through? Ohmed out power and ground on board. Might have missed something. But doubt it. I believe I have PDR and Boot0 and Boot1 properly. Other than the obvious that the board does not work any ideas? Will not connect using ST-Link V2. Where I am shooting myself in the foot? Thanks Wounded in Surrey Dave