Skip to main content
mvi
Associate III
August 18, 2008
Question

Firmware Upgrade Via USART

  • August 18, 2008
  • 12 replies
  • 1833 views
Posted on August 18, 2008 at 09:33

Firmware Upgrade Via USART

    This topic has been closed for replies.

    12 replies

    mvi
    mviAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Hi,

    Im interested in knowing whether its possible to perform firmware upgrades via the USART. Has anyone tried it? Any directional help is appreciated.

    Thanks.

    -Mad D

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Hi mvi,

    Check :

    http://www.st.com/stonline/products/literature/an/13588.pdf

    : STM32F10xxx in-application programming using the USART .

    Enjoy using it. Cheers,

    STOne-32.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Hi ST7,

    keep cool, I will test it in my boards and let you back what is going there. However, when I posted my message by 22-04-2008 at that time the Application note is handling only one device family ( medium density) and the software is working fine :|

    I will let you know soon,

    Cheers,

    STOne-32.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Quote:

    Check :

    http://www.st.com/stonline/products/literature/an/13588.pdf

    : STM32F10xxx in-application programming using the USART .

    Enjoy using it. Cheers,

    I'm not emjoying it at all - it's making me very frustrated!! :|

    The PDF document says,

    Quote:

    To specify the device (High-density or Medium-density) on which the software is to be run, uncomment the relative definition line in the platform_config.h header file:

    //#define USE_STM3210B_EVAL

    //#define USE_STM3210E_EVAL

    but that's rubbish - because the relevant secion of platform_config.h is actually:

    Quote:

    #if !defined (USE_STM3210B_EVAL) && !defined (USE_STM3210E_EVAL)

    //#define USE_STM3210B_EVAL

    #define USE_STM3210E_EVAL

    #endif

    (I would use the 'CODE' tags there, but that seems to be what breaks my post!)

    So any commenting or un-commenting of those lines will be completely ignored if either (or both) of the symbols is defined in the project - which, of course, they are!! :| :|

    The project builds cleanly immediately after downloading it from the ST site, but if the USE_STM3210E_EVAL definition in the project is changed, the build fails - saying it can't find stm32f10x_conf.h :| :| :|

    Even if the project is then restored to exactly as it was from the site, it will not rebuild again - it continues to say that it can't find stm32f10x_conf.h :| :| :| :|

    If it managed to find it the first time, why can't it find it again?? :| :| :| :| :|

    Leaving the definitions alone and changing the Target processor has a similar effect! :| :| :| :| :| :|

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    What's the matter with this forum - why are my posts disappearing?? :|

    [ This message was edited by: st7 on 14-08-2008 16:32 ]

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    The PDF documents (and readme file) state the requirement that the ''user'' application must start at 0x0800_2000.

    I assume that the example projects supplied must do this, but there is no description of how it is done - which is not very helpful when it comes to creating my own application!

    Can you explain precisely what is needed to do this with RIDE7 ?

    Thanks.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Quote:

    The project builds cleanly immediately after downloading it from the ST site, but if the USE_STM3210E_EVAL definition in the project is changed, the build fails - saying it can't find stm32f10x_conf.h

    Found the cause of that - it's a Raisonance idiocy:

    After changing the Project properties, you have to manually save the project (or close & re-open RIDE) before doing a build - otherwise it uses the wrong include path!! :| :|

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Quote:

    it's a Raisonance idiocy:

    After changing the Project properties, you have to manually save the project (or close & re-open RIDE) before doing a build - otherwise it uses the wrong include path!! :| :|

    UPDATE: Raisonance think this problem may be to do with opening a project created with an earlier version of RIDE...

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:31

    Quote:

    I'm not expert of Ride 8-) toolchain,

    So who created the RIDE projects in the download for this App Note?

    I think they need to correct it - I think it's wrong!

    Raisonance also need to fix their IDE!