Skip to main content
reedomneck
Associate III
Apr 10, 2026 11:38 AM UTC
Question

Firmware update stm32u535

Hi All,

I've this requirement, can someone suggest how do I proceed.

I'm using stm32u535 and over usart it's connected to Silicon labs chip. Silicon labs chip has Wi-Fi and I want to update firmware of STM32U535. This silicon labs chip is connected to cloud over Wi-Fi.

 

1 reply

Andrew Neil
Super User
Apr 10, 2026 12:20 PM UTC

So you'll need to use a UART bootloader - either a custom one, or the System Bootloader (in ROM).

 

The STM32 neither knows nor cares what is on the other end of the link, so see:

How can I use an ESP32 to update the firmware of an STM32 from any family

Links to app notes in this reply

 

#FirmwareUpdate #IAP

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.