Skip to main content
sirpak
Associate III
November 28, 2024
Question

Firmware size

Dear Sirs,

Is there a method to calculate the firmware size?

I am using STM32F103R8T6

My flash memory is divided in three blocks:

- Custom boot loader block

- Main application block

- Data block

When the main application is running, it needs to calculate its own size in terms of quantity of bytes in flash.

This is needed in order to calculate the CRC of the firmware.

Some pages at the end of main application block range might not have been erased, so I think I cannot count on 0xFFFFFF presence. Furthermore the firmware might finish with 0xFF.

Maybe the .hex file starts with the program counter initialization, followed by some useful information??

 

Thanks,

Marco

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
November 28, 2024

Can't you use some Linker Script symbols to scope the image size?

Covered on the forum previously. Can also place size in one of the slack vectors in the table so tools can recover. 

Can determine also from object file structures, ie LOADBITS and via what the .HEX touches

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
sirpak
sirpakAuthor
Associate III
November 28, 2024

I need the application to calculate itself or being able to find it somewhere.

I couldn't find previous covering inside the forum.

Pavel A.
November 28, 2024

As @Tesla DeLorean wrote, this is easy with help of the linker script.

For example, append this at the end of the script after the last section:

 

 

 

MEMORY
{
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
.........
}

SECTIONS
{
................
 .flash_end (NOLOAD) : {
 . = ALIGN(4);
 } >FLASH

 my_FLASH_SIZE = (LOADADDR(.flash_end) - ORIGIN(FLASH)) ;
}

 

 

Then, in some .c file:

 

 

extern char my_FLASH_SIZE; // exported by linker script
#define MY_FLASH_SIZE ((size_t)&my_FLASH_SIZE)

 

 

 

> Maybe the .hex file starts with the program counter initialization, followed by some useful information??

No chance. Standard hex files carry no such things.

Andrew Neil
Super User
November 28, 2024

@sirpak wrote:

This is needed in order to calculate the CRC of the firmware


Why?

Why not just calculate the CRC over the entire region of memory dedicated to the application?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
sirpak
sirpakAuthor
Associate III
November 28, 2024

Because when a firmware is programmed, it just erase and program its own pages, not the whole Main application block memory space.

Doing so, there might be leftovers in other pages, if a smaller firmware overwrites a bigger firmware. Those leftovers might differ from device to device.

Andrew Neil
Super User
November 28, 2024

So why not make sure  that it does erase the whole area?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.