Skip to main content
Hemanth Sundaresh
Associate II
Jul 13, 2017 1:57 PM UTC
Solved

FIFO in UART of STM32F767

Posted on July 13, 2017 at 15:57

Hello All,

I wanted to know if the STM32F767, supports FIFO for the UART module? If yes, what is the size.

I need the FIFO details for configuring the Hardware flow control.

regards,

Hemanth

#uart #stm32f7 #fifo
This topic has been closed for replies.
AvaTar
AvaTarBest answer
Senior III
Jul 13, 2017 2:18 PM UTC
Posted on July 13, 2017 at 16:18

I wanted to know if the STM32F767, supports FIFO for the UART module?

No.

ST's Cortex M controllers generally have no FIFO. You can use DMA instead. Actually, you are supposed to use DMA.

Check the Reference Manual.

1 reply

AvaTar
AvaTarBest answer
Senior III
Jul 13, 2017 2:18 PM UTC
Posted on July 13, 2017 at 16:18

I wanted to know if the STM32F767, supports FIFO for the UART module?

No.

ST's Cortex M controllers generally have no FIFO. You can use DMA instead. Actually, you are supposed to use DMA.

Check the Reference Manual.