Skip to main content
hokus
Associate
January 24, 2016
Question

FFT problem

  • January 24, 2016
  • 1 reply
  • 686 views
Posted on January 24, 2016 at 17:45

Hi, I need do FFT on stm32f4 and therefore I

have few questions:

1. Is there any why to directly copy adc values which are uint16_t to float32_t buffer using DMA, without casting them in fork loop and using two buffers. I used this:  

DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

DMA_MemoryDataSize = DMA_MemoryDataSize_Word;

but i get only zeros.

2. I tested  arm_rfft_fast_f32 function from CMSIS-DSP 1.4.4 with generated 50hz sine wave at 1000Hz sample rate using 1024 samples, but i get peek value at 102, not 51 which i should get 1000/1024 ~0,97 * 51 = 50Hz:

uint16_t i;

    float32_t khz10[1024];

    float32_t maxvalue;

    uint32_t maxindex;

    //float32_t output2[1024];

    arm_rfft_fast_instance_f32 S;

    arm_rfft_fast_init_f32(&S, 1024);

    printf(''Input=['');

    for(i=0; i<1024; i++){

        khz10[i] = 1.2f*arm_sin_f32(2*3.1415926f*50*i/1000)+1;

        printf(''%f,'',khz10[i]);

    }

    printf('']\r\n'');

    arm_rfft_fast_f32(&S, khz10,khz10,0);

    arm_abs_f32(khz10, khz10, 1024);

    arm_max_f32(khz10+1, 1023, &maxvalue, &maxindex);

    printf(''Max:[%ld]:%f Output=['',maxindex,maxvalue);

    for(i=0; i<1024; i++){

        printf(''%f,'',khz10[i]);

    }

    printf('']\r\n'');

thx for help

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    January 24, 2016
    Posted on January 24, 2016 at 19:42

    Is there any why to directly copy adc values which are uint16_t to float32_t buffer using DMA

    No, they use an inherently different representation of the data in the bits of the word.

    https://en.wikipedia.org/wiki/Single-precision_floating-point_format

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..