Skip to main content
Associate II
July 12, 2024
Solved

FDCAN2 Rx callback doesn't work STM32H753

Dear all,

I'm struggeling to get FDCAN2 working on my board. I also use FDCAN1 - which is working pretty good.
For FDCAN1 I selected the RxFifo0 and for FDCAN2 I selected RxFifo1.

But for some reasons, I dont get the callback for HAL_FDCAN_RxFifo1Callback().

Thats part of my own code, where I used the _weak function HAL_FDCAN_RxFifo1Callback(

 

 

// CAN 2 receive interrupt callback
void HAL_FDCAN_RxFifo1Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo1ITs)
{

//....

// the incoming message will be used for further scenarios

//...

}

 

I can also see that the interrupt function will not be called for FDCAN2 if I put a breakpoint into this section (FDCAN1 is working as mentioned)

 

void FDCAN2_IT1_IRQHandler(void)
{
 /* USER CODE BEGIN FDCAN2_IT1_IRQn 0 */

 /* USER CODE END FDCAN2_IT1_IRQn 0 */
 HAL_FDCAN_IRQHandler(&hfdcan2);
 /* USER CODE BEGIN FDCAN2_IT1_IRQn 1 */

 /* USER CODE END FDCAN2_IT1_IRQn 1 */
}

 

I also added my .ioc file - much appreciate if you can have a look into this, due I'm running out of ideas how to go ahead.

This topic has been closed for replies.
julredBest answer
Associate II
July 22, 2024

I just got the message from ST - Support.

It is now working after implementing the following function call:

 

HAL_FDCAN_ConfigGlobalFilter(&hfdcan2, FDCAN_ACCEPT_IN_RX_FIFO1, FDCAN_ACCEPT_IN_RX_FIFO1, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE); 

9 replies

mƎALLEm
ST Technical Moderator
July 12, 2024

Hello,

It could be many reasons: interrupt not enabled, Filter not configured correctly, not the correct Rx pin used.. etc ..

I invite you to inspire from this example: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/FDCAN/FDCAN_Com_IT

But first, try loopback mode: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/FDCAN/FDCAN_Loopback

Hope it helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
julredAuthor
Associate II
July 12, 2024

If I configure FDCAN on RxFifo0, then everything is working. So pinsetting etc. is fine.

I will check-out your posted links. Do you have time to investigate into attached ioc file?

mƎALLEm
ST Technical Moderator
July 12, 2024

According to your ioc file, I noticed that you didn't set any of Std/Ext filter numbers. I think you need to set at least one filter for each if you are receiving both types of frames:

 hfdcan.Init.StdFiltersNbr = 1;
 hfdcan.Init.ExtFiltersNbr = 1;

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ST Employee
July 12, 2024

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,
Jake

ST Support

julredAuthor
Associate II
July 16, 2024

Any updates so far?

mƎALLEm
ST Technical Moderator
July 16, 2024

Did you check my last comment?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
julredAuthorBest answer
Associate II
July 22, 2024

I just got the message from ST - Support.

It is now working after implementing the following function call:

 

HAL_FDCAN_ConfigGlobalFilter(&hfdcan2, FDCAN_ACCEPT_IN_RX_FIFO1, FDCAN_ACCEPT_IN_RX_FIFO1, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE); 

mƎALLEm
ST Technical Moderator
July 22, 2024

But, previously, you said "If I configure FDCAN on RxFifo0, then everything is working"

Did you enable that line for FIFO0?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.