Skip to main content
GS1
Senior III
Sep 3, 2025 2:40 PM UTC
Solved

FDCAN with BRS activated: Problem transmitting 64 Bytes on FDCAN

Hi all,

I am trying to use FDCAN with Baud rate switch (500 kB / 2 MBit) activated and I want to send 64 Byte.

Processor is STM32H7A3. Project was set up with CubeMX V. 6.11.1 and HAL FW_H7 V1.11.2. Clock for FDCAN is 80 MHz.

 

The problem is that the system only sends with 500 kB and 8 Bytes only.

I am transmitting the data to my PC using a PEAK USB dongle (FDCAN capable with BRS) and in parallel check the messages on a scope. 

I don't know, why it doesn't switch to 2 MBit and I only see  8 Bytes with 500 kBit on my scope and on PCAN-Explorer.

Here my init and transmit code sequences:

FDCAN_HandleTypeDef* phCan;

phCan = &hfdcan1;
phCan->Instance = FDCAN1;

phCan->Init.Mode = FDCAN_MODE_NORMAL; 
phCan->Init.FrameFormat = FDCAN_FRAME_FD_BRS;

phCan->Init.AutoRetransmission = ENABLE; 
phCan->Init.TransmitPause = DISABLE;

phCan->Init.NominalPrescaler = 10;
phCan->Init.NominalSyncJumpWidth = 1;
phCan->Init.NominalTimeSeg1 = 11;
phCan->Init.NominalTimeSeg2 = 4;

phCan->Init.DataPrescaler = 2;
phCan->Init.DataSyncJumpWidth = 1;
phCan->Init.DataTimeSeg1 = 14;
phCan->Init.DataTimeSeg2 = 5;

phCan->Init.MessageRAMOffset = 0;
phCan->Init.StdFiltersNbr = 0;
phCan->Init.ExtFiltersNbr = 0;

phCan->Init.RxFifo0ElmtsNbr = 16; // 0..64
phCan->Init.RxFifo1ElmtsNbr = 16;
phCan->Init.RxBuffersNbr = 10;

phCan->Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_64;
phCan->Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_64;
phCan->Init.RxBufferSize = FDCAN_DATA_BYTES_64;


phCan->Init.TxEventsNbr = 0;
phCan->Init.TxBuffersNbr = 0;

phCan->Init.TxFifoQueueElmtsNbr = 16;
phCan->Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

phCan->Init.TxElmtSize = FDCAN_DATA_BYTES_64;

phCan->msgRam.StandardFilterSA = 0;
phCan->msgRam.ExtendedFilterSA = 0;
phCan->msgRam.RxFIFO0SA = 0;
phCan->msgRam.RxFIFO1SA = 0;
phCan->msgRam.RxBufferSA = 0;
phCan->msgRam.TxEventFIFOSA = 0;
phCan->msgRam.TxBufferSA = 0;
phCan->msgRam.TxFIFOQSA = 0;
phCan->msgRam.TTMemorySA = 0;
phCan->msgRam.EndAddress = 0;
phCan->ErrorCode = 0;


halErr = HAL_FDCAN_Init(phCan);

halErr = HAL_FDCAN_Start(phCan);

----------------------------------

TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;

TxHeader.FDFormat = FDCAN_FRAME_FD_BRS;
TxHeader.BitRateSwitch = FDCAN_BRS_ON;

TxHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;//FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;

TxHeader.Identifier = 0x55;

TxHeader.DataLength = FDCAN_DLC_BYTES_64;

halErr = HAL_FDCAN_AddMessageToTxFifoQ(phfdcan, &TxHeader, TxData); // TxData = 64 Bytes

Is there anything missing or wrong?

Thank you for any support or hints.

BR GS

Post edited by the ST moderator to follow the community rule especially for the code sharing.

 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 3, 2025 2:57 PM UTC

Hello,

First, please use </> button to share your code. Please refer to this post: How to insert source code

Second, what is your transceiver allowed bitrate bandwidth?

3rd, what is your clock source? HSI or a crystal?

4th, please call the following before the call of HAL_FDCAN_Start():

 /**
 * Configure and enable Tx Delay Compensation, required for BRS mode.
 * TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
 * TdcFilter default recommended value: 0
 */
 if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, (hfdcan1.Init.DataPrescaler * hfdcan1.Init.DataTimeSeg1), 0U) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

19 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 3, 2025 2:57 PM UTC

Hello,

First, please use </> button to share your code. Please refer to this post: How to insert source code

Second, what is your transceiver allowed bitrate bandwidth?

3rd, what is your clock source? HSI or a crystal?

4th, please call the following before the call of HAL_FDCAN_Start():

 /**
 * Configure and enable Tx Delay Compensation, required for BRS mode.
 * TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
 * TdcFilter default recommended value: 0
 */
 if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, (hfdcan1.Init.DataPrescaler * hfdcan1.Init.DataTimeSeg1), 0U) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
GS1
GS1Author
Senior III
Sep 3, 2025 3:39 PM UTC

Hello,

thank you for your help:

- The transceiver is TCAN1042HG and can do up to 5 MBit 

- Clock source for the system is a Crystal 8 MHz, Clocksource for FDCAN is Clock Divider PLL2Q 

- I inserted your code suggestion. However the result is the same as before. Only 8 Byte with 500 kBit arrive

Any other ideas?

 

BR GS

 

 

mƎALLEm
ST Technical Moderator
Sep 3, 2025 4:47 PM UTC

Could you please attach your project? (tomorrow I'm out of office)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
LCE
Principal III
Sep 3, 2025 3:01 PM UTC

Don't you need extended ID for BRS? 
So try IdType = FDCAN_EXTENDED_ID

Not sure though...

GS1
GS1Author
Senior III
Sep 3, 2025 3:40 PM UTC

Hi LCE,

I tried that, but that doesn't solve the problem. It only changes the ID presentation.

 

BR. GS

 

GS1
GS1Author
Senior III
Sep 4, 2025 3:11 PM UTC

Hello,

I am sorry, but I can not send the complete project. We are using our own custom board and the FDCAN part is now a with BRS is a new required feature.

Would the .IOC file be sufficient? Then you could include the posted initialisation and the send routine.

 

Meanwhile I will do some more trials with the latest HAL library, debugging (with Keil ULINKPro), to confirm, that the registers are treated correctly, etc. 

 

BR GS

LCE
Principal III
Sep 4, 2025 3:33 PM UTC

You are setting:

TxHeader.FDFormat = FDCAN_FRAME_FD_BRS;

This is not a valid value, so probably resets TX to BRS off.
I guess you copied from init...

Try setting it to:

TxHeader.FDFormat = FDCAN_FD_CAN;

 

GS1
GS1Author
Senior III
Sep 4, 2025 3:51 PM UTC

Hello LCE,

thank you for pointing this out. You are right! 

I tried that and now this at least changes the behaviour, but not in the direction I expected: Now it doesn't send at all in FDCAN Mode. FIFO gets full and HAL_ERROR is returned when sending further messages. 

 

I will keep on learning and trying...  

BR GS

LCE
Principal III
Sep 8, 2025 9:04 AM UTC

I have often seen, that the sampling point is rather at 80%.

This will depend on the accumulated delays due to the hardware bus structure, mainly due to capacitance.

What are the TDC settings? Although TDC is probably not needed at 2 Mbps.

mƎALLEm
ST Technical Moderator
Sep 8, 2025 9:13 AM UTC

The sampling point is around 80-87% in the arbitration phase. It seems not the case in the data phase. He needs to use Kvaser tool to confirm. I never had more than 60% in data phase with Kvaser tool.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
LCE
Principal III
Sep 8, 2025 9:17 AM UTC

Can the Kvaser tool mimic a heavier bus load, so that other sampling points can be tested / make sense?