Skip to main content
Nickelgrass
Senior
Dec 19, 2024 3:09 PM UTC
Solved

FDCAN interrupt on STM32G481

Hello,

I am using STM32G491 FDCAN modules 1 and 2 in bare metal. While everything works perfectly on CAN2 the interrupt on CAN1 is constantly disabled. And I do not mean the flags but the actual interrupt does not fire. Each time the interrupt for CAN2 fires, the interrupt from CAN1 is disabled. When I read out the register NVIC->ISER[0] after initialization then I can see bits 6 (EXTI0) and 21 (FDCAN1_IT0) are set. Once FDCAN2 interrupt fires these two bits are reset to 0. I need to enable them again in the ISR of CAN2. How can this happen? How can the interrupt simply be disabled by a different interrupt?

This topic has been closed for replies.
Nickelgrass
NickelgrassBest answer
Senior
Dec 19, 2024 3:26 PM UTC

Found the problem. Was unrelated to the interrupt. Why is not possible to delete useless posts?

2 replies

Nickelgrass
NickelgrassAuthorBest answer
Senior
Dec 19, 2024 3:26 PM UTC

Found the problem. Was unrelated to the interrupt. Why is not possible to delete useless posts?

mƎALLEm
ST Technical Moderator
Dec 19, 2024 3:31 PM UTC

Perhaps, put the solution and accept it as solution.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.