Skip to main content
Associate II
Jul 6, 2026 8:14 PM UTC
Solved

FDCAN bus acknowledge

When using the FDCAN peripheral on a STM32H743 or a STM32H753 and the message filters are setup to only accept certain messages, does the FDCAN hardware ACK a valid message that is rejected by the message filter?

Ozone
OzoneBest answer
Principal
Jul 7, 2026 6:50 AM UTC

Yes, always.

Read the CAN specification.
If a message does not get acknowledged, the sending node would go eventually into an error state, and temporarily shuts itself off the bus.
The acknowledge orininates from the CAN peripheral (Bosch IP block), as soon as it receives a valid CAN frame.

The transmission on the physical layer and the internal processing of messages are not tightly coupled.

2 replies

mƎALLEm
ST Technical Moderator
Jul 6, 2026 8:17 PM UTC

Hello,

Not specific to STM32 but to the CAN protocol. The ACK bit is generated automatically by the CAN/FDCAN cell when at least one CAN node has received the frame correctly. By "received the frame" I mean a correct frame not necessarily passing the CAN filters.

Hope I’ve answred your question.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Ozone
OzoneBest answer
Principal
Jul 7, 2026 6:50 AM UTC

Yes, always.

Read the CAN specification.
If a message does not get acknowledged, the sending node would go eventually into an error state, and temporarily shuts itself off the bus.
The acknowledge orininates from the CAN peripheral (Bosch IP block), as soon as it receives a valid CAN frame.

The transmission on the physical layer and the internal processing of messages are not tightly coupled.