Skip to main content
gregstm
Senior II
September 3, 2015
Question

Fast FIR - less than one cycle per tap

Posted on September 03, 2015 at 16:17

Any interest in a block FIR routine (16 bit data) that can execute (on average) 1 tap in less than 1 cycle?

The catch: It is an 8 tap filter (result not rounded).

The filter has low start and end overhead and can be easily cascaded. Calculating coefficients for cascaded sections is a bit of a mystery though. Data block size has to be a multiple of 8.

When I finally get my hands on some STM32L4 hardware I can verify/optimise the load/store cycles and tidy up the code.

Not sure how useful this thing is, but it was certainly good assembly practice.

    This topic has been closed for replies.

    2 replies

    gregstm
    gregstmAuthor
    Senior II
    September 23, 2015
    Posted on September 23, 2015 at 11:46

    Tested and tweaked with actual STM32L4 hardware now. Result: 15 cycles for 16 taps = 0.9374 cycles per tap. So the M4 can be faster than a standard DSP - at least for an 8 tap filter. Will keep researching into how to cascade these things.

    qwer.asdf
    Senior
    September 23, 2015
    Posted on September 23, 2015 at 12:21

    Thank you, surely it'll be interesting to see. It'll be wonderful if you could share the code on GitHub.