Question
Failure when migrating STM32CubeMX project to compatible part
I have tried to migrate an STM32CubeMX project from the STM32H747AIIx to the STM32H747XIHx using the procedure described here:
How to switch from one STM32 to another using STM3... - STMicroelectronics Community
It failed with the following error message:
"Project Import failed: Import 'STM32H747AIIx' not supported (multiple context)"
Any idea what is wrong???
I am using STM32CubeMX v6.11.0 with firmware package STM32Cube FW_H7 V1.11.1, on Windows 11.