Skip to main content
Ajack.1
Associate
May 7, 2024 7:23 AM UTC
Question

Failure modes for STM32HXX Processor

I'm doing an MTTFd, just wondering what the failure modes are for this processor. I.E Outputs stuck high, output

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 7, 2024 7:44 AM UTC

Which processor? Summary says HXX tagged as F0

Things are apt to have millions of gates, bit simplistic to assume pins will just latch up.

Could presumably just stop, output randomly or not even start at all. Not to mention software induced failures.

Would suggest working with your FAE to determine if your application is suitable or a supported business space. And with QA to understand the fault coverage and testing methodology. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..