Skip to main content
Armen Levonian
Visitor II
Nov 23, 2017 7:10 PM UTC
Question

Failing to write to SD card on SensorTile.

Posted on November 23, 2017 at 20:10

I am using the DataLog application to try to write to the SD card on the SensorTile. I have configured main.c:

LogInterface_TypeDef LoggingInterface = SDCARD_Datalog;

...changed from the default ...= USB_Datalog

In debugging the problem, I can see that in DATALOG_SD_Init...

The 'f_mount(&SDFatFs, (TCHAR const*)SDPath, 0)' fails (not equal to FR_OK).

After calling FATFS_LinkDriver(&SD_Driver, SDPath): which returns 0 (success)

SDPath = '0:/'

I am using the latest firmware:

V2.J29.M18 STM32 Debug+Mass storage

I have a 2GB Micro SD card in the SensorTile cradle.

Is anyone else having issues with this?

UPDATE: OK I have the problem solved. I replaced the 2GB SD card with a new 16GB SD card, the the DataLog app is now logging to the SD card. It seems older smaller cards are not supported.

Thanks,

Armen

    This topic has been closed for replies.