Skip to main content
Associate III
June 27, 2023
Question

Failing to flash a new program after writing to memory -- STM32F439 microcontroller

  • June 27, 2023
  • 2 replies
  • 1573 views

Hello everyone, I am running into the following problem when reprogramming after a write to flash memory.

I am unable to reprogram the microcontroller after writing to flash memory.

In my program I write to bank 2 ( address 0x08100000 ) of the microcontroller using:

 

 

HAL_FLASH_Unlock();


EraseInitStruct.TypeErase = TYPEERASE_SECTORS;
EraseInitStruct.Sector = FLASH_SECTOR_12;
EraseInitStruct.NbSectors = 2;
EraseInitStruct.VoltageRange = VOLTAGE_RANGE_3;

HAL_FLASHEx_Erase(&EraseInitStruct, &flash_error_information);



while(update->start_address + update->current_byte_num != update->end_address)
{
HAL_FLASH_Program( FLASH_TYPEPROGRAM_BYTE, update->start_address + update->current_byte_num, update->data_to_write_in_flash[ update->current_byte_num ]);
update->current_byte_num++;
}

HAL_FLASH_Lock();

 

 

 

After running the program and attempting to flash another program, I then get the following error on a message box:

Error message from debugger back end:

Error finishing flash operation

 

The console returns the following:

Error: ST-LINK error (DEV_TARGET_NOT_HALTED)
Encountered Error when opening C:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer

 

 

The only solution I have found is adding a delay such as HAL_Delay(250); after unlocking the flash memory, but this is far from a permanent solution.

Any help would be greatly apreciated.

 

This topic has been closed for replies.

2 replies

Graduate
May 9, 2024

Hi , Iam also facing the same issue, did you found any solution..?

Tesla DeLorean
Guru
May 9, 2024

Is the code you put in the second bank bad, partial, corrupt?

The System Loader will try to identify second-bank code at 0x08100000

Does behaviour change if you put it deeper ? say 0x08110000 ?

Can you access the device with BOOT0 = HIGH ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..