Skip to main content
AFink.1
Visitor II
March 8, 2025
Question

Failed to execute MI command STM32WBA5

hi

just update STM32CubeIDE  to Version: 1.18.0

And I can't program my Target as before.

getting this error :

Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\user\\STM32CubeIDE\\workspace_1.16.0\\PiezoPump-2\\Debug\\PiezoPump-2.elf

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode: Disabled

Logging Level: 1

Listen Port Number: 61234

Status Refresh Delay: 15s

Verbose Mode: Disabled

SWD Debug: Enabled

InitWhile: Enabled

 

Target not halted after reset. Force halt

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

 

STM32CubeProgrammer v2.19.0

 

 

Error: Unable to connect to the target device, Access port is invalid.

Encountered Error when opening C:\ST\STM32CubeIDE_1.16.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

 

BUT...if I am using the stand-alone STM32CubeProgrammer V2.19.0 I can connect to Target as well as to program.

but using the seam elf fike on STM32CubeIDE led to an error as mentioned above.

please help.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
March 8, 2025

Hello @AFink.1 

Are you using the NUCLEO-WBA55? If so, are you using the NUCLEO-64-Mezzanine board MB1801- NoUSB-D02?

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.