Skip to main content
Julien M
Associate II
Jul 19, 2017 2:05 PM UTC
Solved

Failed to erase an STM32F779NIH6 MCU

Posted on July 19, 2017 at 16:05

Hello everybody,

I have some trouble when I want to erase my chip by  sector erase  or mass erase (ST LINK UTILITY with ST LINK dongle)   I obtain  some  dummy bytes after an erase operation like that :

00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 3C 29 00 08 29 21 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 00 00 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 00 00 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 18 08 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

Can I forget something ?

Normaly is filled by 0xFF ?

When I use this method on a STM32F103 it works well.

Of course when I try to put a firmware it become like a random firmware because the flash was not really erased.

Do you have some idea to help me ?

Thank you so much .

Julien.

    This topic has been closed for replies.
    STOne-32
    STOne-32Best answer
    ST Technical Moderator
    Jul 20, 2017 6:09 PM UTC
    Posted on July 20, 2017 at 20:09

    Hi Julien,

    Check all of our Hardware connections on board, including VDDs, VDDAs, VCAP Pins etc.. PDR_ON etc..

    you can monitor VCAP pins with a voltmeter and check the value of ~1.2Volts.   Hope it helps you.

    Cheers,

    STOne-32.

    4 replies

    STOne-32
    STOne-32Best answer
    ST Technical Moderator
    Jul 20, 2017 6:09 PM UTC
    Posted on July 20, 2017 at 20:09

    Hi Julien,

    Check all of our Hardware connections on board, including VDDs, VDDAs, VCAP Pins etc.. PDR_ON etc..

    you can monitor VCAP pins with a voltmeter and check the value of ~1.2Volts.   Hope it helps you.

    Cheers,

    STOne-32.

    Julien M
    Julien MAuthor
    Associate II
    Jul 21, 2017 10:24 AM UTC
    Posted on July 21, 2017 at 10:24

    Hi ,

    Thank you so much for your help,  my power path management  seems to be wrong in my custom board , but in another one it works fine. thank you so much.

    Julien M
    Julien MAuthor
    Associate II
    Jul 21, 2017 3:12 PM UTC
    Posted on July 21, 2017 at 15:12

    Hi, 

    Thank you but I try to test my  other custom board (same batch) and I have some trouble STLINK tool can't erase all the time the board, if I use OpenOCD tools, I can erase sometime but with different time for sector 1  sometime 1 second and sometime 17 seconds and of course when I read again all byte stay in place. (erase failed) . I am so confuse, it is seems to be work but not always.  Power issue  on my schematic ?  But 3.3V not so bad and 1.2V seems to be ok . 1 mistake maybe VCAP are 4.7uF and not 2.2uF do you think than it can be the cause of my issue ?

    And when I succeed to flash correctly, the CPU won't start correctly just 1 time... 

    Thank you so much for your help.

    Thank you community.