Skip to main content
AMull.11
Associate III
February 8, 2021
Question

Facing difficulty to access internal bootloader in STM32H743BIT6

  • February 8, 2021
  • 2 replies
  • 490 views

Hi Guys,

I working on one project where we need to enter into system bootloader for updating new firmware through the UART from software without using BOOT0 Pin.

But I am facing problem in entering bootloader through software(user application).

I had created function to enter bootloader.

I am successfully entering into system bootloader when I directly call the JumpToSystemBootLoader() ,but when I call through HAL_UART_RxCpltCallback I don't see any response from the bootloader (getting error in STM32CubeProg). 

void JumpToSystemBootLoader (void)

{

   void (*JumpToSysBoot)(void); /* declare a function pointer */

__IO uint32_t sys_boot_address = 0; 

uint8_t indx = 0;

sys_boot_address = 0x1FF09800;/* STM32H7 system BootLoader address */

/* Disable all enabled interrupts in NVIC and Clear all pending interrupt requests in NVIC */

for (indx = 0; indx < 8; indx++)

  {

NVIC->ICER[indx] = 0xFFFFFFFF;

     NVIC->ICPR[indx] = 0xFFFFFFFF;

/* Disable all enabled peripherals, use HSI clock */

  HAL_RCC_DeInit();

/* Disable all interrupts */

  __set_PRIMASK(1); 

/* Disable SysTick */

SysTick->CTRL = 0;

 SysTick->LOAD = 0;

 SysTick->VAL = 0;

/* Enable all interrupts */

__set_PRIMASK(0);

JumpToSysBoot = (void (*)(void)) (*((uint32_t *) (sys_boot_address + 4)));

/* Activate the MSP */

 __set_MSP(*(uint32_t *)sys_boot_address);

__set_CONTROL(0);

/* Jump to the system BootLoader */

 JumpToSysBoot(); 

/* It will not execute if jump is successful*/

  while (1)

{

 __NOP();

}

}

Method 1: In this below method, successfully connecting with UART and updating new firmware

int main(void)

{

 while (1)

  {

HAL_UART_Receive(&huart1, (uint8_t*)RxBuffer, 2, 200);

/*If KEY matches with RXBuffer then enter into System bootloader*/

(strcmp(KEY, RxBuffer) == 0)

{

HAL_UART_Transmit(&huart1, (uint8_t*)TxBuffer, strlen(TxBuffer),200);

  JumpToSystemBootLoader();

}

}

}

Method 2: In this below method, didn't getting any response from System bootloader

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)

{

  if (strcmp(BOOT_MODE, RxBuffer) == 0)

{

__HAL_UART_DISABLE_IT(&huart1, UART_IT_RXNE);

HAL_UART_Transmit(&huart1, (uint8_t*)TxBuffer, strlen(TxBuffer),200);

JumpToSystemBootLoader();

}

}

int main(void)

{

__HAL_UART_ENABLE_IT(&huart1, UART_IT_RXNE);

HAL_UART_Receive_IT(&huart1, (uint8_t*)RxBuffer, 2);

 while (1)

  {

}

}

Thank You

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
February 9, 2021

There have been many discussions and proposals for solution in this forum before. Did you scan those posts?

AMull.11
AMull.11Author
Associate III
February 9, 2021

Yeah but I didn't understand properly.

Can you explain me how to solve this issue.

Thank You