Skip to main content
kRaje.1
Associate III
November 7, 2024
Question

Facing an issue with open bootloader on STM32U0

Hi Team,

I am facing an issue regarding the open bootloader. Recently, I downloaded the open bootloader source code for the STM32U0 boards, and I was successfully able to load hex files via the STM32Cube Programmer over UART.

However, I encountered a problem when I try to load hex files with incorrect addresses. Specifically, when I load an application hex file with an incorrect address, the STM32Cube Programmer is erasing my bootloader source code.

For example, when I flash my bootloader source at address 0x8000000 and load an application hex file with the address 0x8000100, everything works as expected and I do not encounter any issues. But if I try to load an application hex file with an incorrect address like 0x8000004, the bootloader source code gets erased.

I have attempted to handle this issue within the bootloader source code, but I am unable to address it from the source code side. Is there a way to prevent this from happening or handle such situations in the bootloader code?

I would appreciate your guidance on how to resolve this issue.

This topic has been closed for replies.

1 reply

ST Technical Moderator
November 7, 2024

Hello @kRaje.1 

Please specify the Cubeprogrammer version you're using.

If possible, please share the hex files used.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks