Skip to main content
waclawek.jan
Super User
January 16, 2018
Question

['F446 documentation] SAI/SPDIF-Tx bit clock formula missing

Posted on January 16, 2018 at 12:02

0690X00000609LJQAY.png
    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    January 16, 2018
    Posted on January 16, 2018 at 12:47

    On second thought - I've seen the formula in other RMs, but IMO that formula ought to be given in terms of SAI signals as defined and SAI registers fields (namely MCLK), as it's different than clocking in free protocol modes (in that FRL is ignored).

    The formula at MCLK's description ought to say so, too.

    JW

    waclawek.jan
    Super User
    January 24, 2018
    Posted on January 24, 2018 at 19:43

    The formula I mentioned above I've seen in 'F7 documentation is wrong anyway:

    0690X00000609TzQAI.png

    as fS is not fSCK_x/64; and certainly not fSAI_CK_x / 64.

    And this is wrong, too:

    0690X00000609N5QAI.png

    as it's not just the input frequency to SAI block, i.e. fSAI_CK_x , which is alone responsible for the resulting sampling frequency.

    The fact is that (denoting the SPDIF symbol rate fSYMB) fS = fSYMB / 64; but fSYMB=fSCK_x / 2.

    And, fSCK_x follows the same rules as in FREE mode, i.e. fSCK_x = fSAI_CK_x if NODIV=1; fSCK_x = fSAI_CK_x / (256 / (FRL+1)) if NODIV=

    1

    0

    [EDIT]was a typo, sorry[/EDIT]

    and MCKDIV=0; and fSCK_x = fSAI_CK_x / ((2 * MCKDIV) * 256 / (FRL+1)) otherwise; where (FRL+1) = 64.

    In other words, the final fS-to-fSAI_SCK_x ratio is half of what would be for the FREE mode with the same NODIV and MCKDIV settings.

    Of course, Cube gets it wrong, too; as it does not account for this factor of half. The only example I could find for SAI in SPDIF-Tx mode (namely in [STM32Cube_FW_F7_V1.7.0]\Projects\STM32F769I-Discovery\Examples\SPDIFRX\SPDIFRX_Loopback\) has no visible/audible output, and uses as receiver the SPDIFRX module, which is adaptive enough to ignore the fact that the output sample rate is half of what was intended.

    JW

    waclawek.jan
    Super User
    March 5, 2018
    Posted on March 05, 2018 at 13:41

    While in the new RM, the formula is there:

    0690X00000609vtQAA.png

    it's only partially true. As I've said above, fSCK_x follows the same formula as in FREE mode, with that the setting in FRL is ignored and is taken as if is fixed (FRL+1)=64.

    Thus:

    if  NODIV=1  fSCK_x = fSAI_CK_x

    If NODIV=0 and MCKDIV=0, fSCK_x = fSAI_CK_x / 4

    If NODIV=0 and MCKDIV>0, fSCK_x = fSAI_CK_x / (8 * MCKDIV)

    JW