Solved
waclawek.janBest answer
Super User
December 27, 2021
> 2) Mega2560 and 16450/16550 support 5 to 9 data bits + parity bit + 1 or 2 stop bits.
ST chose to count the parity bits up to the data bits, which is different from most UARTS there. I was a bad choice, but it is what it is.
> So this would then imply that ST MCU is unable to do start + 9 data bits + parity bit + stop bit(s)?
Yes.
JW