Skip to main content
MM..1
Super User
Mar 11, 2024 2:13 PM UTC
Question

F4 HAL CRC utility

Hi , have somebody link to exe or online or linux utility with same result as HAL CRC calculate?

 

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
Mar 11, 2024 2:19 PM UTC

srecord

JW

MM..1
MM..1Author
Super User
Mar 11, 2024 2:22 PM UTC

Thanks srec line example for bin file ?

Tesla DeLorean
Guru
Mar 11, 2024 2:35 PM UTC

https://community.st.com/t5/stm32-mcus-products/stm32f4-crc32-algorithm-headache/m-p/371428

https://community.st.com/t5/stm32-mcus-security/crc-computation/m-p/536190/page/2

// STM32 CRC32 Test App - sourcer32@gmail.com
// Copyright (C) 2014

#include <windows.h>
#include <stdio.h>
#include <stdlib.h>

//****************************************************************************

DWORD Crc32(DWORD Crc, DWORD Data)
{
 int i;
 Crc = Crc ^ Data;
 for(i=0; i<32; i++)
 if (Crc & 0x80000000)
 Crc = (Crc << 1) ^ 0x04C11DB7; // Polynomial used in STM32
 else
 Crc = (Crc << 1);
 return(Crc);
}

//****************************************************************************

DWORD Crc32Block(DWORD Crc, DWORD Size, DWORD *Buffer) // 32-bit units
{
 while(Size--)
 Crc = Crc32(Crc, *Buffer++);

 return(Crc);
}

//****************************************************************************

DWORD Crc32Fast(DWORD Crc, DWORD Data)
{
 static const DWORD CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial
 0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005,
 0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD };

 Crc = Crc ^ Data; // Apply all 32-bits

 // Process 32-bits, 4 at a time, or 8 rounds
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];

 return(Crc);
}

//****************************************************************************

DWORD Crc32FastBlock(DWORD Crc, DWORD Size, DWORD *Buffer) // 32-bit units
{
 while(Size--)
 Crc = Crc32Fast(Crc, *Buffer++);

 return(Crc);
}

//****************************************************************************

void test(void)
{
 BYTE vector[12] = { 0x02,0x07,0x02,0x00,0x18,0x8A,0xD0,0x23,0x25,0x2B,0x09,0x00 }; // ACD7E298
 DWORD Crc;
 int i;

 for(i=0; i<sizeof(vector); i++)
 printf("%02X ",vector[i]);
 putchar('\n');

 Crc = 0xFFFFFFFF; // Initial state

 for(i=0; i<sizeof(vector); i+=4)
 {
 Crc = Crc32Fast(Crc, *((DWORD *)&vector[i]) ); // 4-bytes at a time
 }

 printf("%08X %08X test",Crc, Crc32FastBlock(0xFFFFFFFF, sizeof(vector)/4, (void *)vector));
}

//****************************************************************************

void TestFile(char *Filename)
{
 FILE *f;
 DWORD Size;
 BYTE *Buffer;

 f = fopen (Filename, "rb");
 if (f)
 {
 fseek(f, 0, SEEK_END);

 Size = ftell (f);

 fseek(f, 0, SEEK_SET);

 if (Size & 3)
 printf("WARNING: File must be multiple of 4 bytes (32-bit) for valid results\n");

 Buffer = malloc(Size);

 fread(Buffer, Size, 1, f);

 fclose(f);

 printf("crc=%08X Slow\n", Crc32Block(0xFFFFFFFF, Size >> 2, (void *)Buffer));
 printf("crc=%08X Fast", Crc32FastBlock(0xFFFFFFFF, Size >> 2, (void *)Buffer));

 free(Buffer);
 }
 else
 printf("ERROR: Unable to open file '%s'\n", Filename);
}

//****************************************************************************

int main(int argc, char **argv)
{
 printf("STM32CRC Test\n Usage: STM32CRC [<file>]\n");

 if ((Crc32(0xFFFFFFFF, 0x12345678) != 0xDF8A8A2B) ||
 (Crc32Fast(0xFFFFFFFF, 0x12345678) != 0xDF8A8A2B))
 {
 printf("ERROR: Internal Sanity Check Failed\n");
 }

 if (argc > 1)
 TestFile(argv[1]);
 else
 test();

 return(1);
}

//****************************************************************************
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MM..1
MM..1Author
Super User
Mar 11, 2024 3:56 PM UTC

Thanks i compile it on linux after little complication with DWORD. Now it work and result is same thx.

But for other is better have utility ready...

Tesla DeLorean
Guru
Mar 11, 2024 5:28 PM UTC

Not exactly rocket sciencery..  but I'll bite.

windows.h contained DWORD

https://github.com/cturvey/RandomNinjaChef/blob/main/stm32crc.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Mar 11, 2024 6:35 PM UTC

I looked at RandomNinjaChef's menu first, but couldn't find the right flavour of CRC there.

Oh, it's a fresh dish.

JW