Question
F3/L4 ADC in Differential mode.
Posted on May 30, 2017 at 17:44
Hi,
When two inputs of ADC are in differential mode, can the ADCxINN input voltage be higher than the ADCxINP input voltage?
For Vref+ = 3.3V and Verf- = 0V.
Is the result value = ((ADCxINP - ADCxINN)/3.3) * 2048 + 2048?
Ex. If ADCxINP = 1.0V and ADCxINN = 2.65V, is the result value = 1024?
Ari.