f_write is giving FR_DISK_ERROR
Hi STM community,
I am working with STM32F779i board , using system workbench for stm IDE. in my project I am using freertos ,fatfs ,sdcard drivers and CAN drivers. Initially as per project requirement we need more RAM, so we have implemented SDRAM as RAM.
We have two tasks , one for fatfs and another for CAN . I am receiving a file from PC over CAN and writing it to a buffer(buffer size is sizeof file created with malloc) on to SDRAM, another task is waiting till we received whole file over CAN and then I am writing the buffer to file in the SDCARD .
I am able to write small files(10kB, 40KB) successfully,But for large files (more than > 50KB) the f_write is returning FR_DISK_ERR.
I dig into the f_write function and it is failing at below ABORT(fs, FR_DISK_ERR);
and the value of clst is 0xFFFFFFFF;
{
clst = create_chain(&fp->obj, fp->clust); /* Follow or stretch cluster chain on the FAT */ } } if (clst == 0) break; /* Could not allocate a new cluster (disk full) */ if (clst == 1) ABORT(fs, FR_INT_ERR); if (clst == 0xFFFFFFFF) ABORT(fs, FR_DISK_ERR);}
Can anyone tell me why which case I will get this error ?
and how to resolve this error ?
#stm32f7-eval