EXTI0 Falling Edge Triggered by Button on PD0 but not PA0
I am having an issue with triggering interrupts with anything other than a button (that sinks to ground when pressed) with an external pullup on port D. I have another line (PA0) on my board that gets pulled low on USB plug-in and uses in internal (rather than external) pull-up. It is not being used for an alternate function. It is completely dedicated as an input in the same way that I have configured the button lines (Fun fact, you can use a single line as both an interrupt and a polled input if you configure it as an interrupt). I observe with a multimeter that the line does indeed go low on plug-in (3.2 to zero volts). I also poll this line to see that it has gone low in order to provide power via USB, which works. This is leading me to believe that I am doing something wrong in software that isn't allowing me to detect the interrupt. I perform the following in code to configure PA0 (the line that doesn't get interrupts)
//Enable the syscfg Clock
__HAL_RCC_SYSCFG_CLK_ENABLE();
/* Configure Enable Source pin as input */
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING; //was GPIO_MODE_INPUT GPIO_MODE_IT_FALLING
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Set Enable Source Interrupt priority */
HAL_NVIC_SetPriority(EXTI0_IRQn, 9, 0);
/* Enable Enable Source Interrupt */
HAL_NVIC_EnableIRQ(EXTI0_IRQn);I also perform the following in code to configure my button lines (which work).
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING; //was GPIO_MODE_INPUT GPIO_MODE_IT_FALLING
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* Set CenterButton Interrupt priority */
HAL_NVIC_SetPriority(EXTI0_IRQn, 9, 0);
/* Enable CenterButton Interrupt */
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
/* Set CenterButton Interrupt priority */
HAL_NVIC_SetPriority(EXTI1_IRQn,9, 0);Even when I configure the PA0 line as an interrupt and not the PD0 line, I still do not get the interrupt. Does anyone see something wrong here?
I also have an important related question, can you configure two pin 0 lines to provide EXTI0? As you can see, I would like to have both PA0 and PD0 acting as external interrupts.
Thanks!
Zach