Skip to main content
LPola
Associate II
Sep 10, 2019 5:41 AM UTC
Solved

EXTI pins located at which port pins of STM32H753ZI MCU?

Hi team,

I would like to use the external interrupt for handling peripherals, but i didn't find the exact port pin of MCU. for example EXTI0 is an external interrupt pin which is located at?

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Sep 10, 2019 8:58 AM UTC

Yes, unless the given pin is set to Analog mode.

SYSCFG_EXTICR1.EXTI0 is specifically for EXTI0, other EXTI have their respective fields in other SYSCFG_EXTICRx registers, refer to the SYSCFG chapter in RM.

JW

7 replies

waclawek.jan
Super User
Sep 10, 2019 5:52 AM UTC

PA0, or PB0, or PC0, etc., as selected by SYSCFG_EXTICR1.EXTI0.

JW

LPola
LPolaAuthor
Associate II
Sep 10, 2019 6:29 AM UTC

Thank you.

1) In PA0 : The alternate functionalites are TIM2_CH1/TIM2_ETR, TIM5_CH1, TIM8_ETR, TIM15_BKIN, USART2_CTS/USART2_ NSS, UART4_TX, SDMMC2_CMD, SAI2_SD_B, ETH_MII_CRS, EVENTOUT.

Additional Functions are ADC1_INP16, WKUP0.

2) In PB0 : The alternate functionalites are TIM1_CH2N, TIM3_CH3, TIM8_CH2N, DFSDM1_CKOUT, UART4_CTS, LCD_R3, OTG_HS_ULPI_D1, ETH_MII_RXD2, LCD_G1, EVENTOUT

Additional Functions are ADC12_INN5, ADC12_INP9, OPAMP1_VINP, COMP1_INP.

3) In PC0 : The alternate functionalites are DFSDM1_CKIN0, DFSDM1_DATIN4, SAI2_FS_B, OTG_HS_ULPI_STP, FMC_SDNWE, LCD_R5, EVENTOUT.

Additional Functions are ADC123_ INP10.

Of these multi functionalities which of them is external interrupt?

LPola
LPolaAuthor
Associate II
Sep 10, 2019 6:28 AM UTC

!

waclawek.jan
Super User
Sep 10, 2019 7:47 AM UTC

> Of these multi functionalities which of them is external interrupt?

None; external interrupt is independent from the alternate functions, and can be used simultaneously with them.

JW

LPola
LPolaAuthor
Associate II
Sep 10, 2019 7:51 AM UTC

Thank you,

You mean to use the concept of external interrupt we can connect to any of the pins and can be configured by using the registers you specified SYSCFG_EXTICR1.EXTI0?

waclawek.jan
waclawek.janBest answer
Super User
Sep 10, 2019 8:58 AM UTC

Yes, unless the given pin is set to Analog mode.

SYSCFG_EXTICR1.EXTI0 is specifically for EXTI0, other EXTI have their respective fields in other SYSCFG_EXTICRx registers, refer to the SYSCFG chapter in RM.

JW

LPola
LPolaAuthor
Associate II
Sep 10, 2019 9:08 AM UTC

Thank you so much.