Skip to main content
Arno Thiele
Associate II
Jan 24, 2018 7:27 PM UTC
Solved

EXTI handler gets stuck

Posted on January 24, 2018 at 20:27

With my STM32F4 I am trying to use an external interrupt to read aquadrature encoder on PC02 and regular port PC The interrupt on PC02 fires when I move the encoder, but it won’t return to the main loop again and my main routine gets stuck. Here’s the code:

init()
{
GPIO_InitTypeDef gpio_init;
EXTI_InitTypeDef exti_init;
NVIC_InitTypeDef nvic_init;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

gpio_init.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
gpio_init.GPIO_Speed = GPIO_Medium_Speed;
gpio_init.GPIO_Mode = GPIO_Mode_IN;
gpio_init.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOC, &gpio_init);

SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOC, EXTI_PinSource2);
exti_init.EXTI_Line = EXTI_Line2;
exti_init.EXTI_LineCmd = ENABLE;
exti_init.EXTI_Mode = EXTI_Mode_Interrupt;
exti_init.EXTI_Trigger = EXTI_Trigger_Falling;
EXTI_Init(&exti_init);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);
nvic_init.NVIC_IRQChannel = EXTI2_IRQn;
nvic_init.NVIC_IRQChannelPreemptionPriority = 0;
nvic_init.NVIC_IRQChannelSubPriority = 0;
nvic_init.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&nvic_init);
}
————————————————————————————————————

void EXTI2_IRQHandler(void) 
{
 if (EXTI_GetITStatus(EXTI_Line2) != RESET) 
 {
 // whatever…
 EXTI_ClearITPendingBit(EXTI_Line2);
 }
}

int main(void)
{
 SystemInit();
 Encoder.init();
while(1)
{}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

In my main loop I am speaking to some periphery over SPI, a DAC, ADC, LED-driver. No matter what I try the IRQHandler gets stuck. Even with no code at all in it. No matter what I remove from my main loop, it’s the same result. It seems like the pending bit of the EXTI line don’t get cleared but it is obviously cleared in the handler in line

I tried calling the interrupt in software to look at it in my debugger but there it just skips back to the main loop with no problems.

I know I can use the encoder function of the timers and I got it to work just fine, but I need 8 encoders in total so they are all taken already.

Any advice would be appreciated!

    This topic has been closed for replies.
    Jan Waclawek
    Jan WaclawekBest answer
    Visitor II
    Jan 25, 2018 7:54 AM UTC
    Posted on January 25, 2018 at 08:54

    Is this C++? Isn't the ISR name mangled?

    JW

    2 replies

    Jan Waclawek
    Jan WaclawekBest answer
    Visitor II
    Jan 25, 2018 7:54 AM UTC
    Posted on January 25, 2018 at 08:54

    Is this C++? Isn't the ISR name mangled?

    JW

    Arno Thiele
    Associate II
    Jan 25, 2018 3:30 PM UTC
    Posted on January 25, 2018 at 16:30

    Thank you Sir, you spotted it correctly! 

    I forgot to turn off the name mangling by running the IRQ handler with <extern 'C'> in front.