https://github.com/cturvey/stm32extldr/blob/main/h7_w25q128/CLIVEONE-W25Q128_STM32H7XX-PB2-PB10-PD11-PD12-PE2-PA1.stldr
This loader was built with Keil, but attached is the GNU Linker Script I used in other H7 Loader projects
/*
*****************************************************************************
**
** File : ExternalLoader.ld
**
** Abstract : Linker script for STM32H7xx Device with
** 2048KByte FLASH, 128KByte RAM
**
** Copyright (c) 2020-2021 Clive One / sourcer32@gmail.com
**
*****************************************************************************
*/
/* Entry Point */
ENTRY(Init)
/* Specify the memory areas */
MEMORY
{
RAM_INFO (r) : ORIGIN = 0, LENGTH = 1K
RAM_PROG (xrw) : ORIGIN = 0x24000004, LENGTH = 128K-4 /* 0x20000004 for Non-H7 */
}
/* Define output sections */
SECTIONS
{
.info :
{
KEEP (*(.rodata.StorageInfo))
} >RAM_INFO
/* The program code and other data goes into IMAGE */
.prog :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
/* Ensure entry points are pulled in here */
KEEP (*(.text.Init))
KEEP (*(.text.DeInit))
KEEP (*(.text.Write))
KEEP (*(.text.Read))
KEEP (*(.text.Verify))
KEEP (*(.text.Checksum))
KEEP (*(.text.SectorErase))
KEEP (*(.text.MassErase))
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} >RAM_PROG
/* Constant data goes into IMAGE */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >RAM_PROG
.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} >RAM_PROG
.ARM :
{
*(.ARM.exidx*)
} >RAM_PROG
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} >RAM_PROG
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} >RAM_PROG
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} >RAM_PROG
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
*(.data) /* .data sections */
*(.data*) /* .data* sections */
. = ALIGN(4);
} >RAM_PROG
/* Uninitialized data section */
.bss :
{
. = ALIGN(4);
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
} >RAM_PROG
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..