Associate II
Mar 17, 2021 9:22 AM UTC
Solved
External interruption flag not detected - Nucleo64 -STM32F091RC
- 2 replies
- 987 views
Hello,
I am working on Flighing sensors VL53L3 and I would like to run them in interrupt mode.
But my board (Nucleo-64 STM32F091RC) doesn't detect any flag in the falling edge trigger.
I have already run this interrupt mode on another board and this worked well.
I also tried to set the interruption pin on the user Button and that's work perfectly!
Moreover, I checked with a logic analyzer if the sensor set down rightly the interruption wire and it is the case.
I saw on different forums that it's could be a memory issue or a clock one but I have any ideas to debug my issue...
I will attach my project folder (I am working with AC6 tools for STM32).
Thanks for future help