Skip to main content
Richard Tarbell_2
Associate II
August 25, 2017
Question

External FLASH for F765 with the FMC

  • August 25, 2017
  • 0 replies
  • 1250 views
Posted on August 25, 2017 at 15:09

Greetings All!

In the past, we have used the F4 series (F427) with the FMC memory controller, to interface with 2GB of external NANDFLASH memory.  This worked with no problems.

NOW, we have the same setup (same wiring and connections), except that we are using the F765 micro.  When reading certain memory locations of the Flash, we get faulty/bad data, such as 0xFFFFFFFF when we know it should read something else.  We have played with different values for the memory timing (setup/hold/etc.) parameters, with no success.

--> Are there any known issues, specifically with the FMC on the F7 series?

#nand-flash #fmc #f7
This topic has been closed for replies.