Skip to main content
Associate III
Jun 2, 2025 3:08 PM UTC
Solved

External clock requirement on N6 Family

Hello,

 

I was wondering about the reasons to supply external clocks to the N6 MCU, since it seems that via HSI and LSI there are clocks integrated into the MCU.

 

I am having trouble to understand whether the internal clocks can satisfy my requirements:

- I don't have special accuracy requirements for LSE/LSI nor HSI/HSE

- I am using the CSI-2 interface

- I am using SPI and UART Interface

 

Are there reasons to supply external clocks?

Are there other considerations that I might have to take into account? (especially for example considering data rates of the interfaces that I am using or other)

 

Best Regards

Lucas

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 2, 2025 4:41 PM UTC

Generally it's things like Ethernet, USB and CAN which have critical timing expectations / standards.

Async UART does not, and can tolerate several percent error. Synchronous, where you provide the clocking, like SPI or camera sources, providing a clock, also generally safe.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 2, 2025 4:41 PM UTC

Generally it's things like Ethernet, USB and CAN which have critical timing expectations / standards.

Async UART does not, and can tolerate several percent error. Synchronous, where you provide the clocking, like SPI or camera sources, providing a clock, also generally safe.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..