Skip to main content
hashtala
Associate III
August 28, 2020
Question

exporting Keil debugger values from registers to PC without UART

Hello

When debugging, I obviously use ST-Link and Keil displays register values for me

Can I export these values somehow without having to transmit them over UART?

I need these values for later graphing in python and UART would just take unnecessary scripting, is there any other way?

Thanks

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
August 28, 2020

Not something I've tried to do with Keil.

What interfaces does your board support/provide?

For the F7, you could use the SWO pin to implement SWV (Serial Wire Viewer), I can cut-n-paste that from a window in Keil

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
August 28, 2020

You can use SWO instead.

Still going to need the script to turn them into a plot.

STM32CubeMonitor can monitor and plot variables in real-time. Could try that.

"Live Expressions" in STM32CubeIDE will update expressions as they change.

"If you feel a post has answered your question, please click ""Accept as Solution""."