Skip to main content
Phillips Jr..Clyde
Associate III
Jun 17, 2014 9:59 PM UTC
Question

EWARM St-Link debug of STM32F4 Discovery board not using .intvec

Posted on June 17, 2014 at 23:59

The PC is always pointing to 0x08000188 (after the .intvec allotment )

So as a workaround I put a B <label> there. The label value is incorrect.

This is not using the flash loader. If I use it it fails citing writes to the CCM area.

All the generic STM32F4 manual don't mention the 0x08000000 as even being in the memory map. And i can't set the intvec to flash load at 0x0.

Is there information about these issues anywhere?

Thanks Clyde

    This topic has been closed for replies.

    15 replies

    Tesla DeLorean
    Guru
    Jun 20, 2014 4:01 AM UTC
    Posted on June 20, 2014 at 06:01

    The linker appears to be describing a 46685 byte region at 0x10000000, that appears to be zeros and loading. Where as the region at 0x20000000 has no data behind it.

    ...
     Section Header #4
    sh_name 0000001B (A1 rw)
    sh_type 00000001 (***_PROGBITS)
    sh_flags 00000006 (-AX)
    sh_addr 08000000
    sh_offset 00000034
    sh_size 00000188
    sh_link 00000000
    sh_info 00000000
    sh_addralign 00000004
    sh_entsize 00000001
    Section Header #5
    sh_name 00000021 (P1 ro)
    sh_type 00000001 (***_PROGBITS)
    sh_flags 00000006 (-AX)
    sh_addr 08000188
    sh_offset 000001BC
    sh_size 0000020C
    sh_link 00000000
    sh_info 00000000
    sh_addralign 00000004
    sh_entsize 00000001
    Section Header #6
    sh_name 00000027 (P2 rw)
    sh_type 00000001 (***_PROGBITS)
    sh_flags 00000003 (WA-)
    sh_addr 10000000
    sh_offset 000003C8
    sh_size 0000B65D
    sh_link 00000000
    sh_info 00000000
    sh_addralign 00000004
    sh_entsize 00000001
    Section Header #7
    sh_name 0000002D (A2 rw)
    sh_type 00000008 (***_NOBITS)
    sh_flags 00000003 (WA-)
    sh_addr 2000E000
    sh_offset 0000BA28
    sh_size 00002000
    sh_link 00000000
    sh_info 00000000
    sh_addralign 00000008
    sh_entsize 00000001
     ... 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Phillips Jr..Clyde
    Associate III
    Jun 20, 2014 4:43 AM UTC
    Posted on June 20, 2014 at 06:43

    Yes I allocate all 64k of the CCM at 0x10000000. I use DC32 to increment the address counter for the labels I use. The SRAM1 and SRAM2 would not be used by my code until run-time.

    The memory being allocated this way has not been a problem. I can flash my code and play with my memory on several other boards. And this code runs in this chips simulator. It's only 40 - 50 lines of assembly code. Load registers to fill CCM with a pattern, initialize 12 words and bomb. All I need of the ST-Link debugger is to run the code after it downloads it.

    The code loads but then the ST-Link quits with two error messageboxes, showing the message ''Writing outside flash memory at address 0x10000000''

    My code is small and not doing this! Can I omit the section and still have my labels link?

    Do I need to hand calculate and code the labels I reference in my code? Allocating in .noninit for label addresses is what I'm doing here. Am I doing it wrong~)

    Thanks, Clyde

    Tesla DeLorean
    Guru
    Jun 20, 2014 10:52 AM UTC
    Posted on June 20, 2014 at 12:52

    The problem seems to be with what the linker does, the ST-LINK is just programming the portions it was directed, the J-LINK might recognize the regions as Cortex-Mx memory, but the issue is in the .ELF(OUT) file.

    I don't use IAR much, but I think the issue can be resolved in the .ICF file the linker is processing. I'm not sure it recognizes ''.noinit'' as a magic section, it needs attributes, and you could name it anything you wanted as long as the linker script was coherent with the naming.

    I think this line would be appropriate:

    do not initialize  { section .noinit };
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Phillips Jr..Clyde
    Associate III
    Jun 20, 2014 9:30 PM UTC
    Posted on June 20, 2014 at 23:30

    I tried all the do do not initialize stuff and renamimng the sections etc and none fixed it. If  a section is declared the linker will force you to ''place'' it.

    So I thought I had solved the problem by not declaring a section. This places all the DCxx allotments in flash which won't work. But it loads w/o error!.

    It is looking like ST-Link a mishandling of  any section that is in RAM...

    Is there a way to strip the section out after the link so the download is fooled?

    Or set the here ( . ) pointer so the DC allot without a SECTION declaration?

    Phillips Jr..Clyde
    Associate III
    Jun 23, 2014 8:40 PM UTC
    Posted on June 23, 2014 at 22:40

    This thread can be closed! I made a rooky mistake and added a few DCx ''variables'' where what I meant was DSx. The DCx created constants that were inappropriate for Ram ( .bss .noinit, etc )

    Fixed this and download and debug working fine!

    Clyde