Skip to main content
Abhishek Anand
Associate II
June 4, 2018
Question

Ethernet Layer 2 Broadcast

Posted on June 04, 2018 at 20:29

Hello Everyone,

I need help to send data packets on Ethernet but i want to broadcast it to all the other device on network. For now i want to send hardcoded data which later could be changed. In STMcubeMx i've checked Ethernet, RCC and SYS. Do i need to add any middleware for Layer 2 broadcast? I'm confused with all the API's provided and couldn't figure out a proper way to do it. I'm using STM32F2207ZG(Nucleo-144). Any sort of help is appreciated. Thank You.

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    June 5, 2018
    Posted on June 05, 2018 at 14:59

    Hello

    abhishek.anand

    ,

    Have a look at this

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM001047pdf/files/DM001047pdf/jcr:content/translations/en.DM001047pdf

    user manual, in paragraph 'B.3.6 LwIP' for the STM32CubeMX LwIP configuration side.

    You'll probably want to review Ethernet application available in the STM32CubeF2 firmware package:

    STM32Cube_FW_F2_V1.7.0\Projects\STM32F207ZG-Nucleo\Applications\LwIP.

    Hope this bring you some help.

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Abhishek Anand
    Associate II
    June 6, 2018
    Posted on June 06, 2018 at 17:33

    Hey

    DAHMEN.IMEN

    ‌,

    Thank You very much for your help but I guess LwIP middleware is used if i'm trying to assign an ip to my board or want it to work with TCP/IP protocols, correct me if i'm wrong i'm new to this? But what i'm trying to do is to send an ethernet packet just using the mac address assigned to mydevkit and flood all the other devices on the network using destination address ff:ff:ff:ff:ff:ff. I don't want to assign any ip address to my board i want to transfer ethernet packet just by the mac address(Mac address broadcast). Do i need to include LwIP for this?

    Abhishek Anand
    Associate II
    June 5, 2018
    Posted on June 05, 2018 at 16:09

    Thank You

    DAHMEN.IMEN

    ‌, that helps.